Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message.
More...
#include <AESCCM.h>
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message.
§ key
A previously initialized CryptoKey
§ aad
uint8_t* AESCCM_Operation_::aad |
A buffer of length aadLength
containing additional authentication data to be authenticated/verified but not encrypted/decrypted.
§ input
uint8_t* AESCCM_Operation_::input |
- Encryption: The plaintext buffer to be encrypted and authenticated in the CCM operation.
- Decryption: The ciphertext to be decrypted and verified.
§ output
uint8_t* AESCCM_Operation_::output |
- Encryption: The output ciphertext buffer that the encrypted plaintext is copied to.
- Decryption: The plaintext derived from the decrypted and verified ciphertext is copied here.
§ nonce
uint8_t* AESCCM_Operation_::nonce |
A buffer containing a nonce. Nonces must be unique to each CCM operation and may not be reused. If nonceInternallyGenerated is set the nonce will be generated by this function call and copied to this buffer.
§ mac
uint8_t* AESCCM_Operation_::mac |
- Encryption: The buffer where the message authentication code is copied.
- Decryption: The buffer containing the received message authentication code.
§ aadLength
size_t AESCCM_Operation_::aadLength |
Length of aad
in bytes. Either aadLength
or plaintextLength
must benon-zero. encrypted.
§ inputLength
size_t AESCCM_Operation_::inputLength |
Length of the input and output in bytes. Either aadLength
or inputLength
must be non-zero.
§ nonceLength
uint8_t AESCCM_Operation_::nonceLength |
Length of nonce
in bytes. Valid nonce lengths are [7, 8, ... 13].
§ macLength
uint8_t AESCCM_Operation_::macLength |
Length of mac
in bytes. Valid MAC lengths are [0, 1, ... 16].
§ nonceInternallyGenerated
bool AESCCM_Operation_::nonceInternallyGenerated |
When true, the nonce buffer passed into the AESCCM_setupEncrypt() and AESCCM_oneStepEncrypt() functions will be overwritten with a randomly generated nonce. Not supported by all implementations.
The documentation for this struct was generated from the following file: