Data Structures | Macros | Typedefs | Enumerations
ECDSACC26X2.h File Reference

Detailed Description

ECDSA driver implementation for the CC26X2 family.

============================================================================

This file should only be included in the board file to fill the ECDSA_config struct.

Hardware and Implementation Details

The CC26X2 family has a dedicated public key accelerator. It is capable of multiple mathematical operations including dedicated ECC point addition, doubling, and scalar multiplication. Only one operation can be carried out on the accelerator at a time. Mutual exclusion is implemented at the driver level and coordinated between all drivers relying on the accelerator. It is transparent to the application and only noted ensure sensible access timeouts are set.

The large number maths engine (LNME) uses a dedicated 2kB block of RAM (PKA RAM) for its operations. The operands of the maths operations must be copied into and results out of the PKA ram. This necessitates a significant number of reads and writes for each operation. The bus interface to the RAM only allows for word-aligned reads and writes. The CPU splits the reads and writes from and to general SRAM from unaligned addresses into multiple bus operations while accumulating the data in a register until it is full. The result of this hardware process is that providing buffers such as plaintext CryptoKey keying material to ECC APIs that are word-aligned will significantly speed up the operation and reduce power consumption.

The driver implementation does not perform runtime checks for most input parameters. Only values that are likely to have a stochastic element to them are checked (such as whether a driver is already open). Higher input paramter validation coverage is achieved by turning on assertions when compiling the driver.

Supported Curve Types

The driver implementation supports the following curve types for ECDSA:

Curve Type Supported
Short Weierstrass Yes
Montgomery No
Edwards No

Public Key Validation

When performing signature verification, the foreign public key will always be validated. However, the implementation assumes that the cofactor, h, of the curve is 1. This lets us skip the computationally expensive step of multiplying the foreign key by the order and checking if it yields the point at infinity. When the cofactor is 1, this property is implied by validating that the point is not already the point at infinity and that it validates against the curve equation. All curves supplied by default, the NIST and Brainpool curves, have cofactor = 1. While the implementation can use arbitrary curves, you should verify that any other curve used has a cofactor of 1.

#include <stdint.h>
#include <stdbool.h>
#include <ti/drivers/Power.h>
#include <ti/drivers/ECDSA.h>
#include <ti/drivers/cryptoutils/ecc/ECCParams.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKey.h>
#include <ti/drivers/dpl/HwiP.h>
#include <ti/drivers/dpl/SwiP.h>
#include <ti/drivers/dpl/SemaphoreP.h>

Go to the source code of this file.

Data Structures

struct  ECDSACC26X2_HWAttrs_
 ECDSACC26X2 Hardware Attributes. More...
 
struct  ECDSACC26X2_Object_
 ECDSACC26X2 Object. More...
 

Macros

#define ECDSACC26X2_STATUS_FSM_RUN_PKA_OP   ECDSA_STATUS_RESERVED - 0
 
#define ECDSACC26X2_STATUS_FSM_RUN_FSM   ECDSA_STATUS_RESERVED - 1
 

Typedefs

typedef enum ECDSACC26X2_FsmState_ ECDSACC26X2_FsmState
 ECDSACC26X2 Sign and Verify states. More...
 
typedef int_fast16_t(* ECDSACC26X2_stateMachineFxn) (ECDSA_Handle handle)
 ECDSACC26X2 state machine function prototype. More...
 
typedef struct ECDSACC26X2_HWAttrs_ ECDSACC26X2_HWAttrs
 ECDSACC26X2 Hardware Attributes. More...
 
typedef struct ECDSACC26X2_Object_ ECDSACC26X2_Object
 ECDSACC26X2 Object. More...
 

Enumerations

enum  ECDSACC26X2_FsmState_ {
  ECDSACC26X2_FSM_ERROR = 0, ECDSACC26X2_FSM_SIGN_VALIDATE_PMSN, ECDSACC26X2_FSM_SIGN_COMPUTE_R, ECDSACC26X2_FSM_SIGN_COMPUTE_R_RESULT,
  ECDSACC26X2_FSM_SIGN_R_MOD_N, ECDSACC26X2_FSM_SIGN_R_MOD_N_RESULT, ECDSACC26X2_FSM_SIGN_COMPUTE_PMSN_INVERSE, ECDSACC26X2_FSM_SIGN_COMPUTE_PMSN_INVERSE_RESULT,
  ECDSACC26X2_FSM_SIGN_COMPUTE_PRIVATE_KEY_X_R, ECDSACC26X2_FSM_SIGN_COMPUTE_PRIVATE_KEY_X_R_RESULT, ECDSACC26X2_FSM_SIGN_ADD_HASH, ECDSACC26X2_FSM_SIGN_ADD_HASH_RESULT,
  ECDSACC26X2_FSM_SIGN_MULT_BY_PMSN_INVERSE, ECDSACC26X2_FSM_SIGN_MULT_BY_PMSN_INVERSE_RESULT, ECDSACC26X2_FSM_SIGN_MOD_N, ECDSACC26X2_FSM_SIGN_MOD_N_RESULT,
  ECDSACC26X2_FSM_VERIFY_R_S_IN_RANGE, ECDSACC26X2_FSM_VERIFY_VALIDATE_PUBLIC_KEY, ECDSACC26X2_FSM_VERIFY_COMPUTE_S_INV, ECDSACC26X2_FSM_VERIFY_COMPUTE_S_INV_RESULT,
  ECDSACC26X2_FSM_VERIFY_MULT_S_INV_HASH, ECDSACC26X2_FSM_VERIFY_MULT_S_INV_HASH_RESULT, ECDSACC26X2_FSM_VERIFY_S_INV_MULT_HASH_MOD_N, ECDSACC26X2_FSM_VERIFY_S_INV_MULT_HASH_MOD_N_RESULT,
  ECDSACC26X2_FSM_VERIFY_MULT_G, ECDSACC26X2_FSM_VERIFY_MULT_G_RESULT, ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R, ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_RESULT,
  ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_MOD_N, ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_MOD_N_RESULT, ECDSACC26X2_FSM_VERIFY_MULT_PUB_KEY, ECDSACC26X2_FSM_VERIFY_MULT_PUB_KEY_RESULT,
  ECDSACC26X2_FSM_VERIFY_ADD_MULT_RESULTS, ECDSACC26X2_FSM_VERIFY_ADD_MULT_RESULTS_RESULT, ECDSACC26X2_FSM_VERIFY_POINTX_MOD_N, ECDSACC26X2_FSM_VERIFY_POINTX_MOD_N_RESULT,
  ECDSACC26X2_FSM_VERIFY_COMPARE_RESULT_R
}
 ECDSACC26X2 Sign and Verify states. More...
 

Macro Definition Documentation

§ ECDSACC26X2_STATUS_FSM_RUN_PKA_OP

#define ECDSACC26X2_STATUS_FSM_RUN_PKA_OP   ECDSA_STATUS_RESERVED - 0

§ ECDSACC26X2_STATUS_FSM_RUN_FSM

#define ECDSACC26X2_STATUS_FSM_RUN_FSM   ECDSA_STATUS_RESERVED - 1

Typedef Documentation

§ ECDSACC26X2_FsmState

ECDSACC26X2 Sign and Verify states.

The sign and verify operations are implemented using multiple invidividual PKA operations. Since state transitions for these operations are almost always predictable, the state transitions are encoded linearly in this enum. The FSM controller will increment the state counter and iterate through states until it is told to stop or restart.

§ ECDSACC26X2_stateMachineFxn

typedef int_fast16_t(* ECDSACC26X2_stateMachineFxn) (ECDSA_Handle handle)

ECDSACC26X2 state machine function prototype.

The FSM controller in the ECDSACC26X2 SWI executes a state machine function containing a switch statement that governs state execution. This function pointer is stored in the object at the beginning of the transaction. This way, unused state machines are removed at link time.

§ ECDSACC26X2_HWAttrs

ECDSACC26X2 Hardware Attributes.

ECDSACC26X2 hardware attributes should be included in the board file and pointed to by the ECDSA_config struct.

§ ECDSACC26X2_Object

ECDSACC26X2 Object.

The application must not access any member variables of this structure!

Enumeration Type Documentation

§ ECDSACC26X2_FsmState_

ECDSACC26X2 Sign and Verify states.

The sign and verify operations are implemented using multiple invidividual PKA operations. Since state transitions for these operations are almost always predictable, the state transitions are encoded linearly in this enum. The FSM controller will increment the state counter and iterate through states until it is told to stop or restart.

Enumerator
ECDSACC26X2_FSM_ERROR 
ECDSACC26X2_FSM_SIGN_VALIDATE_PMSN 
ECDSACC26X2_FSM_SIGN_COMPUTE_R 
ECDSACC26X2_FSM_SIGN_COMPUTE_R_RESULT 
ECDSACC26X2_FSM_SIGN_R_MOD_N 
ECDSACC26X2_FSM_SIGN_R_MOD_N_RESULT 
ECDSACC26X2_FSM_SIGN_COMPUTE_PMSN_INVERSE 
ECDSACC26X2_FSM_SIGN_COMPUTE_PMSN_INVERSE_RESULT 
ECDSACC26X2_FSM_SIGN_COMPUTE_PRIVATE_KEY_X_R 
ECDSACC26X2_FSM_SIGN_COMPUTE_PRIVATE_KEY_X_R_RESULT 
ECDSACC26X2_FSM_SIGN_ADD_HASH 
ECDSACC26X2_FSM_SIGN_ADD_HASH_RESULT 
ECDSACC26X2_FSM_SIGN_MULT_BY_PMSN_INVERSE 
ECDSACC26X2_FSM_SIGN_MULT_BY_PMSN_INVERSE_RESULT 
ECDSACC26X2_FSM_SIGN_MOD_N 
ECDSACC26X2_FSM_SIGN_MOD_N_RESULT 
ECDSACC26X2_FSM_VERIFY_R_S_IN_RANGE 
ECDSACC26X2_FSM_VERIFY_VALIDATE_PUBLIC_KEY 
ECDSACC26X2_FSM_VERIFY_COMPUTE_S_INV 
ECDSACC26X2_FSM_VERIFY_COMPUTE_S_INV_RESULT 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_HASH 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_HASH_RESULT 
ECDSACC26X2_FSM_VERIFY_S_INV_MULT_HASH_MOD_N 
ECDSACC26X2_FSM_VERIFY_S_INV_MULT_HASH_MOD_N_RESULT 
ECDSACC26X2_FSM_VERIFY_MULT_G 
ECDSACC26X2_FSM_VERIFY_MULT_G_RESULT 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_RESULT 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_MOD_N 
ECDSACC26X2_FSM_VERIFY_MULT_S_INV_R_MOD_N_RESULT 
ECDSACC26X2_FSM_VERIFY_MULT_PUB_KEY 
ECDSACC26X2_FSM_VERIFY_MULT_PUB_KEY_RESULT 
ECDSACC26X2_FSM_VERIFY_ADD_MULT_RESULTS 
ECDSACC26X2_FSM_VERIFY_ADD_MULT_RESULTS_RESULT 
ECDSACC26X2_FSM_VERIFY_POINTX_MOD_N 
ECDSACC26X2_FSM_VERIFY_POINTX_MOD_N_RESULT 
ECDSACC26X2_FSM_VERIFY_COMPARE_RESULT_R 
Copyright 2018, Texas Instruments Incorporated