CC26xx Driver Library
rfc_CMD_REMOVE_DATA_ENTRY_s Struct Reference

Remove First Data Entry from Queue. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0006. More...
 
uint16_t __dummy0
 
dataQueue_tpQueue
 Pointer to the queue structure from which the entry will be removed. More...
 
uint8_t * pEntry
 Pointer to the entry that was removed. More...
 

Detailed Description

Remove First Data Entry from Queue.

Field Documentation

uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::__dummy0
uint16_t rfc_CMD_REMOVE_DATA_ENTRY_s::commandNo

The command ID number 0x0006.

uint8_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pEntry

Pointer to the entry that was removed.

dataQueue_t* rfc_CMD_REMOVE_DATA_ENTRY_s::pQueue

Pointer to the queue structure from which the entry will be removed.