CC26xx Driver Library
adi.h File Reference
#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_uart.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_ints.h"
#include "../inc/hw_adi.h"
#include "debug.h"
#include "ddi.h"

Macros

#define ADI_SLAVE_REGS   16
 
#define ADI_PROTECT   0x00000080
 
#define ADI_ACK   0x00000001
 
#define ADI_SYNC   0x00000000
 

Functions

static void ADI8RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Write an 8 bit value to a register in an ADI slave. More...
 
static void ADI16RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Write a 16 bit value to 2 registers in the ADI slave. More...
 
static void ADI32RegWrite (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Write a 32 bit value to 4 registers in the ADI slave. More...
 
static uint32_t ADI8RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value of an 8 bit register in the ADI slave. More...
 
static uint32_t ADI16RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value in a 16 bit register. More...
 
static uint32_t ADI32RegRead (uint32_t ui32Base, uint32_t ui32Reg)
 Read the value in a 32 bit register. More...
 
static void ADI8BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Set specific bits in a single 8 bit ADI register. More...
 
static void ADI16BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Set specific bits in 2 x 8 bit ADI slave registers. More...
 
static void ADI32BitsSet (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Set specific bits in 4 x 8 bit ADI slave registers. More...
 
static void ADI8BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint8_t ui8Val)
 Clear specific bits in an 8 bit ADI register. More...
 
static void ADI16BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Val)
 Clear specific bits in two 8 bit ADI register. More...
 
static void ADI32BitsClear (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Val)
 Clear specific bits in four 8 bit ADI register. More...
 
static void ADI4SetValBit (uint32_t ui32Base, uint32_t ui32Reg, bool bWriteHigh, uint8_t ui8Mask, uint8_t ui8Val)
 Set a value on any 4 bits inside an 8 bit register in the ADI slave. More...
 
static void ADI8SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint16_t ui16Mask, uint16_t ui16Val)
 Set a value on any bits inside an 8 bit register in the ADI slave. More...
 
static void ADI16SetValBit (uint32_t ui32Base, uint32_t ui32Reg, uint32_t ui32Mask, uint32_t ui32Val)
 Set a value on any bits inside an 2 x 8 bit register aligned on a half-word (byte) boundary in the ADI slave. More...
 
void SafeHapiVoid (FPTR_VOID_VOID_T fPtr)
 
void SafeHapiAuxAdiSelect (FPTR_VOID_UINT8_T fPtr, uint8_t ut8Signal)