CC26xx Driver Library
rfc_CMD_ADD_DATA_ENTRY_s Struct Reference

Add Data Entry to Queue. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0005. More...
 
uint16_t __dummy0
 
dataQueue_tpQueue
 Pointer to the queue structure to which the entry will be added. More...
 
uint8_t * pEntry
 Pointer to the entry. More...
 

Detailed Description

Add Data Entry to Queue.

Field Documentation

uint16_t rfc_CMD_ADD_DATA_ENTRY_s::__dummy0
uint16_t rfc_CMD_ADD_DATA_ENTRY_s::commandNo

The command ID number 0x0005.

uint8_t* rfc_CMD_ADD_DATA_ENTRY_s::pEntry

Pointer to the entry.

dataQueue_t* rfc_CMD_ADD_DATA_ENTRY_s::pQueue

Pointer to the queue structure to which the entry will be added.