![]() |
![]() |
RF_ratCapture parameter structure. More...
#include <RF.h>
Data Fields | |
RF_RatCallback | callback |
Callback function to be invoked upon a capture event (optional). More... | |
RF_RatHandle | channel |
RF_RatHandle identifies the channel to be allocated. More... | |
RF_RatCaptureSource | source |
Configuration of the event source to cause a capture event. More... | |
RF_RatCaptureMode | captureMode |
Configuration of the mode of event to cause a capture event. More... | |
RF_RatCaptureRepetition | repeat |
Configuration of the channel to be used in single or repeate mode. More... | |
RF_ratCapture parameter structure.
RF_RatCapture parameters are used with the RF_ratCapture() call.
RF_RatCallback RF_RatConfigCapture::callback |
Callback function to be invoked upon a capture event (optional).
RF_RatHandle RF_RatConfigCapture::channel |
RF_RatHandle identifies the channel to be allocated.
RF_RatCaptureSource RF_RatConfigCapture::source |
Configuration of the event source to cause a capture event.
RF_RatCaptureMode RF_RatConfigCapture::captureMode |
Configuration of the mode of event to cause a capture event.
RF_RatCaptureRepetition RF_RatConfigCapture::repeat |
Configuration of the channel to be used in single or repeate mode.