![]() |
![]() |
Stores the client's internal confguration and states. More...
#include <RF.h>
Stores the client's internal confguration and states.
Before RF_open() can be called, an instance of RF_Object must be created where the RF driver can store its internal configuration and states. This object must remain persistent throughout application run-time and must not be modified by the application.
The size of RF_Object can be optimized for single-mode applications by providing a RF_SINGLEMODE
symbol at compilation time. The prebuilt single-mode archive was generated with this symbol defined, hence any project using this archive must also define RF_SINGLEMODE
on project level.