![]() |
![]() |
Modules | |
Status Codes | |
Command Codes | |
Macros | |
#define | SHA2_CMD_RESERVED (32) |
#define | SHA2_STATUS_RESERVED (-32) |
These SHA2 macros are reservations for SHA2.h
#define SHA2_CMD_RESERVED (32) |
Common SHA2_control command code reservation offset. SHA2 driver implementations should offset command codes with SHA2_CMD_RESERVED growing positively
Example implementation specific command codes:
#define SHA2_STATUS_RESERVED (-32) |
Common SHA2_control status code reservation offset. SHA2 driver implementations should offset status codes with SHA2_STATUS_RESERVED growing negatively.
Example implementation specific status codes: