CC26xx Driver Library
[chipinfo.h] Chip Info

Functions

ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV (void)
 Returns bit vector showing supported protocols. More...
 
static bool ChipInfo_SupportsBLE (void)
 Returns true if the chip supports the BLE protocol. More...
 
static bool ChipInfo_SupportsIEEE_802_15_4 (void)
 Returns true if the chip supports the IEEE 802.15.4 protocol. More...
 
static bool ChipInfo_SupportsPROPRIETARY (void)
 Returns true if the chip supports propriatary protocols. More...
 
PackageType_t ChipInfo_GetPackageType (void)
 Returns package type. More...
 
static bool ChipInfo_PackageTypeIs4x4 (void)
 Returns true if this is a 4x4mm chip. More...
 
static bool ChipInfo_PackageTypeIs5x5 (void)
 Returns true if this is a 5x5mm chip. More...
 
static bool ChipInfo_PackageTypeIs7x7 (void)
 Returns true if this is a 7x7mm chip. More...
 
static bool ChipInfo_PackageTypeIsWAFER (void)
 Returns true if this is a wafer sale chip (naked die). More...
 
static bool ChipInfo_PackageTypeIsWCSP (void)
 Returns true if this is a WCSP chip (flip chip). More...
 
static bool ChipInfo_PackageTypeIs7x7Q1 (void)
 Returns true if this is a 7x7 Q1 chip. More...
 
static uint32_t ChipInfo_GetDeviceIdHwRevCode (void)
 Returns the internal chip HW revision code. More...
 
static uint32_t ChipInfo_GetMinorHwRev (void)
 Returns minor hardware revision number. More...
 
static uint32_t ChipInfo_GetUserId (void)
 Returns the 32 bits USER_ID field. More...
 
ChipType_t ChipInfo_GetChipType (void)
 Returns chip type. More...
 
ChipFamily_t ChipInfo_GetChipFamily (void)
 Returns chip family member. More...
 
static bool ChipInfo_ChipFamilyIs_CC13x0 (void)
 Returns true if this chip is member of the CC13x0 family. More...
 
static bool ChipInfo_ChipFamilyIs_CC26x0 (void)
 Returns true if this chip is member of the CC26x0 family. More...
 
static bool ChipInfo_ChipFamilyIs_CC26x0R2 (void)
 Returns true if this chip is member of the CC26x0R2 family. More...
 
static bool ChipInfo_ChipFamilyIs_CC26x1 (void)
 Returns true if this chip is member of the CC26x1 family. More...
 
static bool ChipInfo_ChipFamilyIs_CC13x2_CC26x2 (void)
 Returns true if this chip is member of the CC13x2, CC26x2 family. More...
 
HwRevision_t ChipInfo_GetHwRevision (void)
 Returns chip HW revision. More...
 
static bool ChipInfo_HwRevisionIs_1_0 (void)
 Returns true if HW revision for this chip is 1.0. More...
 
static bool ChipInfo_HwRevisionIs_2_0 (void)
 Returns true if HW revision for this chip is 2.0. More...
 
static bool ChipInfo_HwRevisionIs_GTEQ_2_0 (void)
 Returns true if HW revision for this chip is 2.0 or greater. More...
 
static bool ChipInfo_HwRevisionIs_2_1 (void)
 Returns true if HW revision for this chip is 2.1. More...
 
static bool ChipInfo_HwRevisionIs_GTEQ_2_1 (void)
 Returns true if HW revision for this chip is 2.1 or greater. More...
 
static bool ChipInfo_HwRevisionIs_2_2 (void)
 Returns true if HW revision for this chip is 2.2. More...
 
static bool ChipInfo_HwRevisionIs_GTEQ_2_2 (void)
 Returns true if HW revision for this chip is 2.2 or greater. More...
 
static bool ChipInfo_HwRevisionIs_GTEQ_2_3 (void)
 Returns true if HW revision for this chip is 2.3 or greater. More...
 
static bool ChipInfo_HwRevisionIs_GTEQ_2_4 (void)
 Returns true if HW revision for this chip is 2.4 or greater. More...
 
void ThisLibraryIsFor_CC26x0R2_HaltIfViolated (void)
 Verifies that current chip is CC26x0R2 and never returns if violated. More...
 

Enumerations

enum  ProtocolBitVector_t { PROTOCOL_Unknown = 0, PROTOCOLBIT_BLE = 0x02, PROTOCOLBIT_IEEE_802_15_4 = 0x04, PROTOCOLBIT_Proprietary = 0x08 }
 Enumeration identifying the protocols supported. More...
 
enum  PackageType_t {
  PACKAGE_Unknown = -1, PACKAGE_4x4 = 0, PACKAGE_5x5 = 1, PACKAGE_7x7 = 2,
  PACKAGE_WAFER = 3, PACKAGE_WCSP = 4, PACKAGE_7x7_Q1 = 5
}
 Package type enumeration. More...
 
enum  ChipType_t {
  CHIP_TYPE_Unknown = -1, CHIP_TYPE_CC1310 = 0, CHIP_TYPE_CC1350 = 1, CHIP_TYPE_CC2620 = 2,
  CHIP_TYPE_CC2630 = 3, CHIP_TYPE_CC2640 = 4, CHIP_TYPE_CC2650 = 5, CHIP_TYPE_CUSTOM_0 = 6,
  CHIP_TYPE_CUSTOM_1 = 7, CHIP_TYPE_CC2640R2 = 8, CHIP_TYPE_CC2642 = 9, CHIP_TYPE_unused = 10,
  CHIP_TYPE_CC2652 = 11, CHIP_TYPE_CC1312 = 12, CHIP_TYPE_CC1352 = 13, CHIP_TYPE_CC1352P = 14
}
 Chip type enumeration. More...
 
enum  ChipFamily_t {
  FAMILY_Unknown = -1, FAMILY_CC26x0 = 0, FAMILY_CC13x0 = 1, FAMILY_CC26x1 = 2,
  FAMILY_CC26x0R2 = 3, FAMILY_CC13x2_CC26x2 = 4
}
 Chip family enumeration. More...
 
enum  HwRevision_t {
  HWREV_Unknown = -1, HWREV_1_0 = 10, HWREV_1_1 = 11, HWREV_2_0 = 20,
  HWREV_2_1 = 21, HWREV_2_2 = 22, HWREV_2_3 = 23, HWREV_2_4 = 24
}
 HW revision enumeration. More...
 

Detailed Description

Function Documentation

static bool ChipInfo_ChipFamilyIs_CC13x0 ( void  )
inlinestatic

Returns true if this chip is member of the CC13x0 family.

Returns
Returns true if this chip is member of the CC13x0 family, false otherwise.
413 {
414  return ( ChipInfo_GetChipFamily() == FAMILY_CC13x0 );
415 }
1 means that the chip is a CC13x0 family member.
Definition: chipinfo.h:367
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101

Here is the call graph for this function:

static bool ChipInfo_ChipFamilyIs_CC13x2_CC26x2 ( void  )
inlinestatic

Returns true if this chip is member of the CC13x2, CC26x2 family.

Returns
Returns true if this chip is member of the CC13x2, CC26x2 family, false otherwise.
469 {
471 }
4 means that the chip is a CC13x2, CC26x2 family member.
Definition: chipinfo.h:370
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101

Here is the call graph for this function:

static bool ChipInfo_ChipFamilyIs_CC26x0 ( void  )
inlinestatic

Returns true if this chip is member of the CC26x0 family.

Returns
Returns true if this chip is member of the CC26x0 family, false otherwise.
427 {
428  return ( ChipInfo_GetChipFamily() == FAMILY_CC26x0 );
429 }
0 means that the chip is a CC26x0 family member.
Definition: chipinfo.h:366
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101

Here is the call graph for this function:

static bool ChipInfo_ChipFamilyIs_CC26x0R2 ( void  )
inlinestatic

Returns true if this chip is member of the CC26x0R2 family.

Returns
Returns true if this chip is member of the CC26x0R2 family, false otherwise.

Referenced by ThisLibraryIsFor_CC26x0R2_HaltIfViolated().

441 {
442  return ( ChipInfo_GetChipFamily() == FAMILY_CC26x0R2 );
443 }
3 means that the chip is a CC26x0R2 family (new ROM contents).
Definition: chipinfo.h:369
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101

Here is the call graph for this function:

static bool ChipInfo_ChipFamilyIs_CC26x1 ( void  )
inlinestatic

Returns true if this chip is member of the CC26x1 family.

Returns
Returns true if this chip is member of the CC26x1 family, false otherwise.
455 {
456  return ( ChipInfo_GetChipFamily() == FAMILY_CC26x1 );
457 }
2 means that the chip is a CC26x1 family member.
Definition: chipinfo.h:368
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101

Here is the call graph for this function:

ChipFamily_t ChipInfo_GetChipFamily ( void  )

Returns chip family member.

Returns
Returns ChipFamily_t

Referenced by ChipInfo_ChipFamilyIs_CC13x0(), ChipInfo_ChipFamilyIs_CC13x2_CC26x2(), ChipInfo_ChipFamilyIs_CC26x0(), ChipInfo_ChipFamilyIs_CC26x0R2(), ChipInfo_ChipFamilyIs_CC26x1(), ChipInfo_GetChipType(), and ChipInfo_GetHwRevision().

102 {
103  uint32_t waferId ;
104  ChipFamily_t chipFam = FAMILY_Unknown ;
105 
106  waferId = (( HWREG( FCFG1_BASE + FCFG1_O_ICEPICK_DEVICE_ID ) &
109 
110  if ( waferId == 0xB99A ) {
111  if ( ChipInfo_GetDeviceIdHwRevCode() == 0xB ) {
112  chipFam = FAMILY_CC26x0R2 ;
113  } else {
114  chipFam = FAMILY_CC26x0 ;
115  }
116  }
117 
118  return ( chipFam );
119 }
0 means that the chip is a CC26x0 family member.
Definition: chipinfo.h:366
-1 means that the chip's family member is unknown.
Definition: chipinfo.h:365
3 means that the chip is a CC26x0R2 family (new ROM contents).
Definition: chipinfo.h:369
ChipFamily_t
Chip family enumeration.
Definition: chipinfo.h:364
static uint32_t ChipInfo_GetDeviceIdHwRevCode(void)
Returns the internal chip HW revision code.
Definition: chipinfo.h:278

Here is the call graph for this function:

ChipType_t ChipInfo_GetChipType ( void  )

Returns chip type.

Returns
Returns ChipType_t
128 {
129  ChipType_t chipType = CHIP_TYPE_Unknown ;
131  uint32_t fcfg1UserId = ChipInfo_GetUserId() ;
132  uint32_t fcfg1Protocol = (( fcfg1UserId & FCFG1_USER_ID_PROTOCOL_M ) >>
134 
135  if ( chipFam == FAMILY_CC26x0R2 ) {
136  switch ( fcfg1Protocol ) {
137  case 0x9 :
138  chipType = CHIP_TYPE_CC2640R2 ;
139  break;
140  }
141  }
142 
143  return ( chipType );
144 }
3 means that the chip is a CC26x0R2 family (new ROM contents).
Definition: chipinfo.h:369
static uint32_t ChipInfo_GetUserId(void)
Returns the 32 bits USER_ID field.
Definition: chipinfo.h:320
-1 means that the chip type is unknown.
Definition: chipinfo.h:331
ChipType_t
Chip type enumeration.
Definition: chipinfo.h:330
ChipFamily_t
Chip family enumeration.
Definition: chipinfo.h:364
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101
8 means that this is a CC2640R2 chip.
Definition: chipinfo.h:340

Here is the call graph for this function:

static uint32_t ChipInfo_GetDeviceIdHwRevCode ( void  )
inlinestatic

Returns the internal chip HW revision code.

Returns
Returns the internal chip HW revision code (in range 0-15)

Referenced by ChipInfo_GetChipFamily().

279 {
280  // Returns HwRevCode = FCFG1_O_ICEPICK_DEVICE_ID[31:28]
281  return ( HWREG( FCFG1_BASE + FCFG1_O_ICEPICK_DEVICE_ID ) >> 28 );
282 }
HwRevision_t ChipInfo_GetHwRevision ( void  )

Returns chip HW revision.

Returns
Returns HwRevision_t

Referenced by ChipInfo_HwRevisionIs_1_0(), ChipInfo_HwRevisionIs_2_0(), ChipInfo_HwRevisionIs_2_1(), ChipInfo_HwRevisionIs_2_2(), ChipInfo_HwRevisionIs_GTEQ_2_0(), ChipInfo_HwRevisionIs_GTEQ_2_1(), ChipInfo_HwRevisionIs_GTEQ_2_2(), ChipInfo_HwRevisionIs_GTEQ_2_3(), and ChipInfo_HwRevisionIs_GTEQ_2_4().

153 {
154  HwRevision_t hwRev = HWREV_Unknown ;
155  uint32_t minorHwRev = ChipInfo_GetMinorHwRev() ;
157 
158  if ( chipFam == FAMILY_CC26x0R2 ) {
159  hwRev = (HwRevision_t)(((uint32_t)HWREV_1_0 ) + minorHwRev );
160  }
161 
162  return ( hwRev );
163 }
HwRevision_t
HW revision enumeration.
Definition: chipinfo.h:478
3 means that the chip is a CC26x0R2 family (new ROM contents).
Definition: chipinfo.h:369
-1 means that the chip's HW revision is unknown.
Definition: chipinfo.h:479
ChipFamily_t
Chip family enumeration.
Definition: chipinfo.h:364
ChipFamily_t ChipInfo_GetChipFamily(void)
Returns chip family member.
Definition: chipinfo.c:101
10 means that the chip's HW revision is 1.0
Definition: chipinfo.h:480
static uint32_t ChipInfo_GetMinorHwRev(void)
Returns minor hardware revision number.
Definition: chipinfo.h:296

Here is the call graph for this function:

static uint32_t ChipInfo_GetMinorHwRev ( void  )
inlinestatic

Returns minor hardware revision number.

The minor revision number is set to 0 for the first market released chip and thereafter incremented by 1 for each minor hardware change.

Returns
Returns the minor hardware revision number (in range 0-127)

Referenced by ChipInfo_GetHwRevision().

297 {
298  uint32_t minorRev = (( HWREG( FCFG1_BASE + FCFG1_O_MISC_CONF_1 ) &
301 
302  if ( minorRev >= 0x80 ) {
303  minorRev = 0;
304  }
305 
306  return( minorRev );
307 }
PackageType_t ChipInfo_GetPackageType ( void  )

Returns package type.

Returns
Returns PackageType_t

Referenced by ChipInfo_PackageTypeIs4x4(), ChipInfo_PackageTypeIs5x5(), ChipInfo_PackageTypeIs7x7(), ChipInfo_PackageTypeIs7x7Q1(), ChipInfo_PackageTypeIsWAFER(), and ChipInfo_PackageTypeIsWCSP().

80 {
81  PackageType_t packType = (PackageType_t)((
82  HWREG( FCFG1_BASE + FCFG1_O_USER_ID ) &
85 
86  if (( packType < PACKAGE_4x4 ) ||
87  ( packType > PACKAGE_7x7_Q1 ) )
88  {
89  packType = PACKAGE_Unknown;
90  }
91 
92  return ( packType );
93 }
5 means that this is a 7x7 mm QFN package with Wettable Flanks.
Definition: chipinfo.h:173
PackageType_t
Package type enumeration.
Definition: chipinfo.h:166
-1 means that current package type is unknown.
Definition: chipinfo.h:167
0 means that this is a 4x4 mm QFN (RHB) package.
Definition: chipinfo.h:168
ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV ( void  )

Returns bit vector showing supported protocols.

Returns
Returns ProtocolBitVector_t which is a bit vector indicating supported protocols.

Referenced by ChipInfo_SupportsBLE(), ChipInfo_SupportsIEEE_802_15_4(), and ChipInfo_SupportsPROPRIETARY().

69 {
70  return ((ProtocolBitVector_t)( HWREG( PRCM_BASE + 0x1D4 ) & 0x0E ));
71 }
ProtocolBitVector_t
Enumeration identifying the protocols supported.
Definition: chipinfo.h:99
static uint32_t ChipInfo_GetUserId ( void  )
inlinestatic

Returns the 32 bits USER_ID field.

How to decode the USER_ID filed is described in the Technical Reference Manual (TRM)

Returns
Returns the 32 bits USER_ID field

Referenced by ChipInfo_GetChipType().

321 {
322  return ( HWREG( FCFG1_BASE + FCFG1_O_USER_ID ));
323 }
static bool ChipInfo_HwRevisionIs_1_0 ( void  )
inlinestatic

Returns true if HW revision for this chip is 1.0.

Returns
Returns true if HW revision for this chip is 1.0, false otherwise.
509 {
510  return ( ChipInfo_GetHwRevision() == HWREV_1_0 );
511 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
10 means that the chip's HW revision is 1.0
Definition: chipinfo.h:480

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_2_0 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.0.

Returns
Returns true if HW revision for this chip is 2.0, false otherwise.
523 {
524  return ( ChipInfo_GetHwRevision() == HWREV_2_0 );
525 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
20 means that the chip's HW revision is 2.0
Definition: chipinfo.h:482

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_2_1 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.1.

Returns
Returns true if HW revision for this chip is 2.1, false otherwise.
551 {
552  return ( ChipInfo_GetHwRevision() == HWREV_2_1 );
553 }
21 means that the chip's HW revision is 2.1
Definition: chipinfo.h:483
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_2_2 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.2.

Returns
Returns true if HW revision for this chip is 2.2, false otherwise.
579 {
580  return ( ChipInfo_GetHwRevision() == HWREV_2_2 );
581 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
22 means that the chip's HW revision is 2.2
Definition: chipinfo.h:484

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_GTEQ_2_0 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.0 or greater.

Returns
Returns true if HW revision for this chip is 2.0 or greater, false otherwise.
537 {
538  return ( ChipInfo_GetHwRevision() >= HWREV_2_0 );
539 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
20 means that the chip's HW revision is 2.0
Definition: chipinfo.h:482

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_GTEQ_2_1 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.1 or greater.

Returns
Returns true if HW revision for this chip is 2.1 or greater, false otherwise.
565 {
566  return ( ChipInfo_GetHwRevision() >= HWREV_2_1 );
567 }
21 means that the chip's HW revision is 2.1
Definition: chipinfo.h:483
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_GTEQ_2_2 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.2 or greater.

Returns
Returns true if HW revision for this chip is 2.2 or greater, false otherwise.
593 {
594  return ( ChipInfo_GetHwRevision() >= HWREV_2_2 );
595 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
22 means that the chip's HW revision is 2.2
Definition: chipinfo.h:484

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_GTEQ_2_3 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.3 or greater.

Returns
Returns true if HW revision for this chip is 2.3 or greater, false otherwise.
607 {
608  return ( ChipInfo_GetHwRevision() >= HWREV_2_3 );
609 }
23 means that the chip's HW revision is 2.3
Definition: chipinfo.h:485
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152

Here is the call graph for this function:

static bool ChipInfo_HwRevisionIs_GTEQ_2_4 ( void  )
inlinestatic

Returns true if HW revision for this chip is 2.4 or greater.

Returns
Returns true if HW revision for this chip is 2.4 or greater, false otherwise.
621 {
622  return ( ChipInfo_GetHwRevision() >= HWREV_2_4 );
623 }
HwRevision_t ChipInfo_GetHwRevision(void)
Returns chip HW revision.
Definition: chipinfo.c:152
24 means that the chip's HW revision is 2.4
Definition: chipinfo.h:486

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIs4x4 ( void  )
inlinestatic

Returns true if this is a 4x4mm chip.

Returns
Returns true if this is a 4x4mm chip, false otherwise.
196 {
197  return ( ChipInfo_GetPackageType() == PACKAGE_4x4 );
198 }
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79
0 means that this is a 4x4 mm QFN (RHB) package.
Definition: chipinfo.h:168

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIs5x5 ( void  )
inlinestatic

Returns true if this is a 5x5mm chip.

Returns
Returns true if this is a 5x5mm chip, false otherwise.
210 {
211  return ( ChipInfo_GetPackageType() == PACKAGE_5x5 );
212 }
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79
1 means that this is a 5x5 mm QFN (RSM) package.
Definition: chipinfo.h:169

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIs7x7 ( void  )
inlinestatic

Returns true if this is a 7x7mm chip.

Returns
Returns true if this is a 7x7mm chip, false otherwise.
224 {
225  return ( ChipInfo_GetPackageType() == PACKAGE_7x7 );
226 }
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79
2 means that this is a 7x7 mm QFN (RGZ) package.
Definition: chipinfo.h:170

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIs7x7Q1 ( void  )
inlinestatic

Returns true if this is a 7x7 Q1 chip.

Returns
Returns true if this is a 7x7 Q1 chip, false otherwise.
266 {
267  return ( ChipInfo_GetPackageType() == PACKAGE_7x7_Q1 );
268 }
5 means that this is a 7x7 mm QFN package with Wettable Flanks.
Definition: chipinfo.h:173
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIsWAFER ( void  )
inlinestatic

Returns true if this is a wafer sale chip (naked die).

Returns
Returns true if this is a wafer sale chip, false otherwise.
238 {
239  return ( ChipInfo_GetPackageType() == PACKAGE_WAFER );
240 }
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79
3 means that this is a wafer sale package (naked die).
Definition: chipinfo.h:171

Here is the call graph for this function:

static bool ChipInfo_PackageTypeIsWCSP ( void  )
inlinestatic

Returns true if this is a WCSP chip (flip chip).

Returns
Returns true if this is a WCSP chip, false otherwise.
252 {
253  return ( ChipInfo_GetPackageType() == PACKAGE_WCSP );
254 }
PackageType_t ChipInfo_GetPackageType(void)
Returns package type.
Definition: chipinfo.c:79
4 means that this is a 2.7x2.7 mm WCSP (YFV).
Definition: chipinfo.h:172

Here is the call graph for this function:

static bool ChipInfo_SupportsBLE ( void  )
inlinestatic

Returns true if the chip supports the BLE protocol.

Returns
Returns true if supporting the BLE protocol, false otherwise.
126 {
127  return (( ChipInfo_GetSupportedProtocol_BV() & PROTOCOLBIT_BLE ) != 0 );
128 }
ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV(void)
Returns bit vector showing supported protocols.
Definition: chipinfo.c:68
Bit[1] set, indicates that Bluetooth Low Energy is supported.
Definition: chipinfo.h:101

Here is the call graph for this function:

static bool ChipInfo_SupportsIEEE_802_15_4 ( void  )
inlinestatic

Returns true if the chip supports the IEEE 802.15.4 protocol.

Returns
Returns true if supporting the IEEE 802.15.4 protocol, false otherwise.
140 {
142 }
ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV(void)
Returns bit vector showing supported protocols.
Definition: chipinfo.c:68
Bit[2] set, indicates that IEEE 802.15.4 is supported.
Definition: chipinfo.h:102

Here is the call graph for this function:

static bool ChipInfo_SupportsPROPRIETARY ( void  )
inlinestatic

Returns true if the chip supports propriatary protocols.

Returns
Returns true if supporting propriatary protocols, false otherwise.
154 {
156 }
Bit[3] set, indicates that proprietary protocols are supported.
Definition: chipinfo.h:103
ProtocolBitVector_t ChipInfo_GetSupportedProtocol_BV(void)
Returns bit vector showing supported protocols.
Definition: chipinfo.c:68

Here is the call graph for this function:

void ThisLibraryIsFor_CC26x0R2_HaltIfViolated ( void  )

Verifies that current chip is CC26x0R2 and never returns if violated.

Returns
None

Referenced by SetupTrimDevice().

170 {
172  {
173  while(1)
174  {
175  // This driverlib version is for CC26x0R2 chip
176  // Do nothing - stay here forever
177  }
178  }
179 }
static bool ChipInfo_ChipFamilyIs_CC26x0R2(void)
Returns true if this chip is member of the CC26x0R2 family.
Definition: chipinfo.h:440

Here is the call graph for this function:

Macro Definition Documentation

#define DRIVERLIB_BUILD_CC13X0   1

1 is the driverlib build ID for the cc13x0 driverlib.

#define DRIVERLIB_BUILD_CC13X2_CC26X2   4

4 is the driverlib build ID for the cc13x2_cc26x2 driverlib.

#define DRIVERLIB_BUILD_CC26X0   0

0 is the driverlib build ID for the cc26x0 driverlib.

#define DRIVERLIB_BUILD_CC26X0R2   3

3 is the driverlib build ID for the cc26x0r2 driverlib.

#define DRIVERLIB_BUILD_CC26X1   2

2 is the driverlib build ID for the cc26x1 driverlib.

#define THIS_DRIVERLIB_BUILD   DRIVERLIB_BUILD_CC26X0R2

Define THIS_DRIVERLIB_BUILD, identifying current driverlib build ID.

This driverlib build identifier can be useful for compile time checking/optimization (supporting C preprocessor expressions).

Enumeration Type Documentation

Chip family enumeration.

Enumerator
FAMILY_Unknown 

-1 means that the chip's family member is unknown.

FAMILY_CC26x0 

0 means that the chip is a CC26x0 family member.

FAMILY_CC13x0 

1 means that the chip is a CC13x0 family member.

FAMILY_CC26x1 

2 means that the chip is a CC26x1 family member.

FAMILY_CC26x0R2 

3 means that the chip is a CC26x0R2 family (new ROM contents).

FAMILY_CC13x2_CC26x2 

4 means that the chip is a CC13x2, CC26x2 family member.

364  {
365  FAMILY_Unknown = -1,
366  FAMILY_CC26x0 = 0,
367  FAMILY_CC13x0 = 1,
368  FAMILY_CC26x1 = 2,
369  FAMILY_CC26x0R2 = 3,
371 } ChipFamily_t;
0 means that the chip is a CC26x0 family member.
Definition: chipinfo.h:366
4 means that the chip is a CC13x2, CC26x2 family member.
Definition: chipinfo.h:370
-1 means that the chip's family member is unknown.
Definition: chipinfo.h:365
3 means that the chip is a CC26x0R2 family (new ROM contents).
Definition: chipinfo.h:369
2 means that the chip is a CC26x1 family member.
Definition: chipinfo.h:368
1 means that the chip is a CC13x0 family member.
Definition: chipinfo.h:367
ChipFamily_t
Chip family enumeration.
Definition: chipinfo.h:364
enum ChipType_t

Chip type enumeration.

Enumerator
CHIP_TYPE_Unknown 

-1 means that the chip type is unknown.

CHIP_TYPE_CC1310 

0 means that this is a CC1310 chip.

CHIP_TYPE_CC1350 

1 means that this is a CC1350 chip.

CHIP_TYPE_CC2620 

2 means that this is a CC2620 chip.

CHIP_TYPE_CC2630 

3 means that this is a CC2630 chip.

CHIP_TYPE_CC2640 

4 means that this is a CC2640 chip.

CHIP_TYPE_CC2650 

5 means that this is a CC2650 chip.

CHIP_TYPE_CUSTOM_0 

6 means that this is a CUSTOM_0 chip.

CHIP_TYPE_CUSTOM_1 

7 means that this is a CUSTOM_1 chip.

CHIP_TYPE_CC2640R2 

8 means that this is a CC2640R2 chip.

CHIP_TYPE_CC2642 

9 means that this is a CC2642 chip.

CHIP_TYPE_unused 

10 unused value

CHIP_TYPE_CC2652 

11 means that this is a CC2652 chip.

CHIP_TYPE_CC1312 

12 means that this is a CC1312 chip.

CHIP_TYPE_CC1352 

13 means that this is a CC1352 chip.

CHIP_TYPE_CC1352P 

14 means that this is a CC1352P chip.

330  {
331  CHIP_TYPE_Unknown = -1,
332  CHIP_TYPE_CC1310 = 0,
333  CHIP_TYPE_CC1350 = 1,
334  CHIP_TYPE_CC2620 = 2,
335  CHIP_TYPE_CC2630 = 3,
336  CHIP_TYPE_CC2640 = 4,
337  CHIP_TYPE_CC2650 = 5,
338  CHIP_TYPE_CUSTOM_0 = 6,
339  CHIP_TYPE_CUSTOM_1 = 7,
340  CHIP_TYPE_CC2640R2 = 8,
341  CHIP_TYPE_CC2642 = 9,
342  CHIP_TYPE_unused = 10,
343  CHIP_TYPE_CC2652 = 11,
344  CHIP_TYPE_CC1312 = 12,
345  CHIP_TYPE_CC1352 = 13,
346  CHIP_TYPE_CC1352P = 14
347 } ChipType_t;
13 means that this is a CC1352 chip.
Definition: chipinfo.h:345
9 means that this is a CC2642 chip.
Definition: chipinfo.h:341
0 means that this is a CC1310 chip.
Definition: chipinfo.h:332
5 means that this is a CC2650 chip.
Definition: chipinfo.h:337
-1 means that the chip type is unknown.
Definition: chipinfo.h:331
14 means that this is a CC1352P chip.
Definition: chipinfo.h:346
11 means that this is a CC2652 chip.
Definition: chipinfo.h:343
7 means that this is a CUSTOM_1 chip.
Definition: chipinfo.h:339
3 means that this is a CC2630 chip.
Definition: chipinfo.h:335
1 means that this is a CC1350 chip.
Definition: chipinfo.h:333
6 means that this is a CUSTOM_0 chip.
Definition: chipinfo.h:338
4 means that this is a CC2640 chip.
Definition: chipinfo.h:336
ChipType_t
Chip type enumeration.
Definition: chipinfo.h:330
12 means that this is a CC1312 chip.
Definition: chipinfo.h:344
8 means that this is a CC2640R2 chip.
Definition: chipinfo.h:340
10 unused value
Definition: chipinfo.h:342
2 means that this is a CC2620 chip.
Definition: chipinfo.h:334

HW revision enumeration.

Enumerator
HWREV_Unknown 

-1 means that the chip's HW revision is unknown.

HWREV_1_0 

10 means that the chip's HW revision is 1.0

HWREV_1_1 

10 means that the chip's HW revision is 1.0

HWREV_2_0 

20 means that the chip's HW revision is 2.0

HWREV_2_1 

21 means that the chip's HW revision is 2.1

HWREV_2_2 

22 means that the chip's HW revision is 2.2

HWREV_2_3 

23 means that the chip's HW revision is 2.3

HWREV_2_4 

24 means that the chip's HW revision is 2.4

478  {
479  HWREV_Unknown = -1,
480  HWREV_1_0 = 10,
481  HWREV_1_1 = 11,
482  HWREV_2_0 = 20,
483  HWREV_2_1 = 21,
484  HWREV_2_2 = 22,
485  HWREV_2_3 = 23,
486  HWREV_2_4 = 24
487 } HwRevision_t;
HwRevision_t
HW revision enumeration.
Definition: chipinfo.h:478
23 means that the chip's HW revision is 2.3
Definition: chipinfo.h:485
10 means that the chip's HW revision is 1.0
Definition: chipinfo.h:481
21 means that the chip's HW revision is 2.1
Definition: chipinfo.h:483
-1 means that the chip's HW revision is unknown.
Definition: chipinfo.h:479
20 means that the chip's HW revision is 2.0
Definition: chipinfo.h:482
22 means that the chip's HW revision is 2.2
Definition: chipinfo.h:484
24 means that the chip's HW revision is 2.4
Definition: chipinfo.h:486
10 means that the chip's HW revision is 1.0
Definition: chipinfo.h:480

Package type enumeration.

Note
Packages available for a specific device are shown in the device datasheet.
Enumerator
PACKAGE_Unknown 

-1 means that current package type is unknown.

PACKAGE_4x4 

0 means that this is a 4x4 mm QFN (RHB) package.

PACKAGE_5x5 

1 means that this is a 5x5 mm QFN (RSM) package.

PACKAGE_7x7 

2 means that this is a 7x7 mm QFN (RGZ) package.

PACKAGE_WAFER 

3 means that this is a wafer sale package (naked die).

PACKAGE_WCSP 

4 means that this is a 2.7x2.7 mm WCSP (YFV).

PACKAGE_7x7_Q1 

5 means that this is a 7x7 mm QFN package with Wettable Flanks.

166  {
167  PACKAGE_Unknown = -1,
168  PACKAGE_4x4 = 0,
169  PACKAGE_5x5 = 1,
170  PACKAGE_7x7 = 2,
171  PACKAGE_WAFER = 3,
172  PACKAGE_WCSP = 4,
173  PACKAGE_7x7_Q1 = 5
174 } PackageType_t;
5 means that this is a 7x7 mm QFN package with Wettable Flanks.
Definition: chipinfo.h:173
PackageType_t
Package type enumeration.
Definition: chipinfo.h:166
-1 means that current package type is unknown.
Definition: chipinfo.h:167
4 means that this is a 2.7x2.7 mm WCSP (YFV).
Definition: chipinfo.h:172
3 means that this is a wafer sale package (naked die).
Definition: chipinfo.h:171
1 means that this is a 5x5 mm QFN (RSM) package.
Definition: chipinfo.h:169
0 means that this is a 4x4 mm QFN (RHB) package.
Definition: chipinfo.h:168
2 means that this is a 7x7 mm QFN (RGZ) package.
Definition: chipinfo.h:170

Enumeration identifying the protocols supported.

Note
This is a bit vector enumeration that indicates supported protocols. E.g: 0x06 means that the chip supports both BLE and IEEE 802.15.4
Enumerator
PROTOCOL_Unknown 

None of the known protocols are supported.

PROTOCOLBIT_BLE 

Bit[1] set, indicates that Bluetooth Low Energy is supported.

PROTOCOLBIT_IEEE_802_15_4 

Bit[2] set, indicates that IEEE 802.15.4 is supported.

PROTOCOLBIT_Proprietary 

Bit[3] set, indicates that proprietary protocols are supported.

99  {
100  PROTOCOL_Unknown = 0 ,
101  PROTOCOLBIT_BLE = 0x02,
None of the known protocols are supported.
Definition: chipinfo.h:100
Bit[3] set, indicates that proprietary protocols are supported.
Definition: chipinfo.h:103
Bit[1] set, indicates that Bluetooth Low Energy is supported.
Definition: chipinfo.h:101
ProtocolBitVector_t
Enumeration identifying the protocols supported.
Definition: chipinfo.h:99
Bit[2] set, indicates that IEEE 802.15.4 is supported.
Definition: chipinfo.h:102