TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
l2capSignalEvent_t Struct Reference

#include <l2cap.h>

Public Attributes

osal_event_hdr_t hdr
 L2CAP_SIGNAL_EVENT and status.
 
uint16 connHandle
 connection message was received on
 
uint8 id
 identifier to match responses with requests
 
uint8 opcode
 type of command: L2CAP Signaling Codes (type of commands)
 
l2capSignalCmd_t cmd
 command data
 

Detailed Description

OSAL L2CAP_SIGNAL_EVENT message format. This message is used to deliver an incoming Signaling command up to an upper layer application.


The documentation for this struct was generated from the following file: