TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
l2capSendSduDoneEvt_t Struct Reference

#include <l2cap.h>

Public Attributes

uint16 CID
 Local channel id.
 
uint16 credits
 Local credits.
 
uint16 peerCID
 Peer channel id.
 
uint16 peerCredits
 Peer credits.
 
uint16 totalLen
 Total length of SDU being transmitted.
 
uint16 txLen
 Total number of octets transmitted.
 

Detailed Description

L2CAP_SEND_SDU_DONE_EVT message format. This message is sent to the app when an SDU transmission is completed or aborted.


The documentation for this struct was generated from the following file: