TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
l2capConnectRsp_t Struct Reference

#include <l2cap.h>

Public Attributes

uint16 dstCID
 Represents CID on device receiving request and sending response.
 
uint16 mtu
 Specifies maximum SDU size that can be received on this channel.
 
uint16 mps
 Specifies maximum payload size that can be received on this channel.
 
uint16 initCredits
 Indicates number of LE-frames that peer device can send.
 
uint16 result
 Indicates outcome of connection request: L2CAP Connection Response Result Values.
 

Detailed Description

Connection Response format.


The documentation for this struct was generated from the following file: