TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
gapUpdateLinkParamReqReply_t Struct Reference

#include <gap.h>

Public Attributes

uint16 connectionHandle
 Connection handle of the update.
 
uint16 intervalMin
 Minimum Connection Interval.
 
uint16 intervalMax
 Maximum Connection Interval.
 
uint16 connLatency
 Connection Latency.
 
uint16 connTimeout
 Connection Timeout.
 
uint8 accepted
 TRUE if host accepts parameter update, FALSE otherwise.
 

Detailed Description

Update Link Parameters Request Reply parameters


The documentation for this struct was generated from the following file: