TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
gapSlaveSecurityReqEvent_t Struct Reference

#include <gap.h>

Public Attributes

osal_event_hdr_t hdr
 GAP_MSG_EVENT and status.
 
uint8 opcode
 GAP_SLAVE_REQUESTED_SECURITY_EVENT.
 
uint16 connectionHandle
 Connection Handle.
 
uint8 deviceAddr [6]
 address of device requesting security
 
uint8 authReq
 Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding)
 

Detailed Description

GAP_SLAVE_REQUESTED_SECURITY_EVENT message format. This message is sent to the app when a Slave Security Request is received.


The documentation for this struct was generated from the following file: