TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
gapEstLinkReq_t Struct Reference

#include <gap.h>

Public Attributes

uint8 taskID
 Requesting App/Profile's Task ID.
 
uint8 highDutyCycle
 TRUE to high duty cycle scan, FALSE if not.
 
uint8 whiteList
 Determines use of the white list: GAP White List Options.
 
uint8 addrTypePeer
 Address type of the advertiser: Address Types as defined by BLE Spec.
 
uint8 peerAddr [6]
 Advertiser's address.
 

Detailed Description

Establish Link Request parameters


The documentation for this struct was generated from the following file: