|
TI BLE Stack API Documentation
2.03.01.00
|
#include <gap.h>
Public Attributes | |
| osal_event_hdr_t | hdr |
| GAP_MSG_EVENT and status. | |
| uint8 | opcode |
| GAP_DEVICE_INFO_EVENT. | |
| uint8 | eventType |
| Advertisement Type: GAP Advertising Report Event Types. | |
| uint8 | addrType |
| address type: Address Types as defined by BLE Spec | |
| uint8 | addr [6] |
| Address of the advertisement or SCAN_RSP. | |
| int8 | rssi |
| Advertisement or SCAN_RSP RSSI. | |
| uint8 | dataLen |
| Length (in bytes) of the data field (evtData) | |
| uint8 * | pEvtData |
| Data field of advertisement or SCAN_RSP. | |
GAP_DEVICE_INFO_EVENT message format. This message is sent to the app during a Device Discovery Request, when a new advertisement or scan response is received.
1.8.12