TI BLE Stack API Documentation  2.03.01.00
Public Attributes | List of all members
attPacket_t Struct Reference

#include <att.h>

Public Attributes

uint8 sig
 Authentication Signature status (not included (0), valid (1), invalid (2))
 
uint8 cmd
 Command Flag.
 
uint8 method
 Method.
 
uint16 len
 Length of Attribute Parameters.
 
uint8 * pParams
 Attribute Parameters.
 

Detailed Description

Attribute Protocol PDU format.


The documentation for this struct was generated from the following file: