TI BLE Stack API Documentation  2.03.00
Public Attributes | List of all members
l2capPsmInfo_t Struct Reference

#include <l2cap.h>

Public Attributes

uint16 mtu
 Maximum SDU size that can be received by local device.
 
uint16 mps
 Maximum payload size that can be received by local device.
 
uint16 initPeerCredits
 Number of LE-frames that peer device can send.
 
uint16 peerCreditThreshold
 Low threshold for number of peer credits.
 
uint8 maxNumChannels
 Maximum number of CO Channels supported by PSM.
 
uint8 numActiveChannels
 Number of active CO Channels.
 

Detailed Description

PSM information format.


The documentation for this struct was generated from the following file: