TI BLE Stack API Documentation  2.03.00
Public Attributes | List of all members
gapAdvertisingParams_t Struct Reference

#include <gap.h>

Public Attributes

uint8 eventType
 Advertise Event Type: GAP Advertising Event Types.
 
uint8 initiatorAddrType
 Initiator's address type: Address Types as defined by BLE Spec.
 
uint8 initiatorAddr [B_ADDR_LEN]
 Initiator's addr - used only with connectable directed eventType (ADV_EVTTYPE_CONNECTABLE_DIRECTED).
 
uint8 channelMap
 Channel Map: Bit mask GAP Advertisement Channel Map.
 
uint8 filterPolicy
 Filer Policy: GAP Advertiser Filter Scan Parameters. Ignored when directed advertising is used.
 

Detailed Description

Advertising Parameters


The documentation for this struct was generated from the following file: