Z-Stack 3.0.1 to Z-Stack 3.1.0¶
This section will describe a way to migrate a project from Z-Stack 3.0.1 to a Z-Stack 3.1.0 project.
For this guide, SampleLight from Z-Stack 3.0.1 will be ported
over to Z-Stack 3.1.0. The two releases are vastly divergent due to differences
in both device and RTOS support, as is covered in CC253x to CC26x2.
The recommended approach is to start with a Z-Stack 3.1.0 project that contains
the same base application as the porting target project and merge any custom functionality
Choose a Z-Stack 3.1.0 example project that contains your target project’s base functionality. For reference and use in this example,
zc_lightfromC:\Texas Instruments\<SimpleLink SDK Path>\examples\rtos\CC26X2R1_LAUNCHXL\zstackis chosen as a starting point.No changes are required for the Z-Stack 3.1.0
zcl_samplelight_data.cfile unless clusters, attributes, or simple descriptors were added or altered in the Z-Stack 3.0.1 project.In
zcl_samplelight.h,bdb_tlCommissioning.hhas been renamedbdb_tl_commissioning.hand/* * Application task entry point for the ZStack Sample Light Application */ extern void zclSampleLight_task(NVINTF_nvFuncts_t *pfnNV);
is used in place of
/* * Initialization for the task */ extern void zclSampleLight_Init( byte task_id ); /* * Event Process for the task */ extern UINT16 zclSampleLight_event_loop( byte task_id, UINT16 events );
Additions may also be necessary for the Application Events, note that Green Power Data Request events have been added to Z-Stack 3.1.0.
Do not copy the Z-Stack 3.0.1
OSAL_SampleLight.cfile and only make changes to the following lines ofmain.c#include "zcl_samplelight.h" /* Kick off application */ zclSampleLight_task(&zstack_user0Cfg.nvFps);
if the task name has been changed inside of
zcl_samplelight.c
The following items specifically concern zcl_samplelight.c:
Note the following changes due to the TI-RTOS implementation:
- ICALL framework used to dispatch messages between Z-Stack and the application
- Semaphores used to post and pend during event callbacks
- Timer handling, i.e
Timer_setTimeout( LevelControlClkHandle, 100 ); Timer_start(&LevelControlClkStruct);
versus
osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT, 100 );. Due to this and the reasons further provided below, all related code from Z-Stack 3.0.1 should not be transferred to the Z-Stack 3.1.0 project.Key events are now handled locally in
zclSampleLight_processKeyinstead ofUI_MainStateMachinefromzcl_sampleapps_ui.c. A UART interface is preferred over LCD.main.ccalls thezclSampleLight_taskfunctionvoid zclSampleLight_task(NVINTF_nvFuncts_t *pfnNV) { // Save and register the function pointers to the NV drivers pfnZdlNV = pfnNV; zclport_registerNV(pfnZdlNV, ZCL_PORT_SCENE_TABLE_NV_ID); // Initialize application zclSampleLight_initialization(); // No return from task process zclSampleLight_process_loop(); }
to initialize the application
static void zclSampleLight_initialization(void) { /* Initialize user clocks */ zclSampleLight_initializeClocks(); /* Initialize keys */ Board_Key_initialize(zclSampleLight_changeKeyCallback); /* Initialize the LEDS */ Board_Led_initialize(); // Register the current thread as an ICall dispatcher application // so that the application can send and receive messages. ICall_registerApp(&zclSampleLight_Entity, &sem); //Initialize stack zclSampleLight_Init(); }
which in-turn initializes the clocks, keys, LEDs, and ICall dispatcher before initializing the stack. This is compared with Z-Stack 3.0.1 where all of the above was accomplished solely in
zclSampleLight_Init.zclSampleLight_Initregisters endpoints using//Register Endpoint zclSampleLightEpDesc.endPoint = SAMPLELIGHT_ENDPOINT; zclSampleLightEpDesc.simpleDesc = &zclSampleLight_SimpleDesc; zclport_registerEndpoint(zclSampleLight_Entity, &zclSampleLightEpDesc);
instead of
// Register the Simple Descriptor for this application bdb_RegisterSimpleDescriptor( &zclSampleLight_SimpleDesc );
and registers applications with
// Register the Application to receive the unprocessed Foundation command/response messages zclport_registerZclHandleExternal(zclSampleLight_ProcessIncomingMsg);
as compared to
// Register the Application to receive the unprocessed Foundation command/response messages zcl_registerForMsg( zclSampleLight_TaskID );
Furthermore, bdb initialization parameters and ZDO callbacks are set up outside of
UI_Init//Write the bdb initialization parameters zclSampleLight_initParameters(); //Setup ZDO callbacks SetupZStackCallbacks();
zclSampleLight_process_loopis used in place ofzclSampleLight_event_loopand uses ICall to receive messages instead ofSYS_EVENT_MSGevents andosal_msg_receivezclSampleLight_processZStackMsgsandzclSampleLight_processAfIncomingMsdIndis used in place ofzclSampleLight_ProcessIncomingMsgDifferent APIs are used for BDB. For example, the
BDB_COMMISSIONING_FORMATIONcase inside ofzclSampleLight_ProcessCommissioningStatusis handled usingzstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq; //After formation, perform nwk steering again plus the remaining commissioning modes that has not been process yet zstack_bdbStartCommissioningReq.commissioning_mode = BDB_COMMISSIONING_MODE_NWK_STEERING | bdbCommissioningModeMsg->bdbRemainingCommissioningModes; Zstackapi_bdbStartCommissioningReq(zclSampleLight_Entity,&zstack_bdbStartCommissioningReq);
when it was previously
//After formation, perform nwk steering again plus the remaining commissioning modes that has not been process yet bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING | bdbCommissioningModeMsg->bdbRemainingCommissioningModes);
Structure type
zclIncomingMsg_thas been renamedzclIncoming_tAdd any other Z-Stack 3.0.1 application changes to the Z-Stack 3.1.0 file if not pertaining to the items listed above
Note
Difference comparison software is recommended for discerning all differences between software stacks.