Zigbee Network Processor (ZNP) Interface

Description

The Z-Stack ZNP is a cost-effective, low power, ZigBee Network Processor that provides full ZigBee functionality with a minimal development effort.

In this solution, the ZigBee PRO stack runs on a SoC and the application runs on an external microcontroller. The Z-Stack ZNP handles all the ZigBee protocol tasks, and leaves the resources of the application microcontroller free to handle the application.

This makes it easy for users to add ZigBee to new or existing products at the same time as it provides great flexibility in choice of microcontroller.

Z-Stack ZNP interfaces to any microcontroller through a range of serial interfaces.

image0

Acronyms

AF ZigBee Application Framework
API Application Programming Interface
AREQ Asynchronous Request
BDB Base Device Behavior
CTS Clear To Send
FCS Frame Check Sequence
GP Green Power
GPIO General Purpose I/O
NPI Network Processor Interface
NV Non-Volatile
PA/LNA Power Amplifier / Low Noise Amplifier (CC259x)
RTS Ready To Send
SoC System on Chip
SREQ Synchronous request
SRSP Synchronous response
UART Universal Asynchronous Receiver Transmitter
ZDO ZigBee Device Object
ZNP ZigBee Network Processor

1. Introduction

This document consolidates the ZNP Interface Specifications for the following devices of the Zigbee® SimpleLink family: CC26X2R1.

To reduce duplicated and redundant information, simple summaries are provided here and references to external documents are provided where necessary.

2. Physical Interface

The following sections describe the physical interface for the ZNP for each of the supported platforms.

2.1 CC26X2R1

2.1.1 Network processor signals

The figure below shows how an application processor interfaces with the CC26X2R1.

image1

Figure 1 : CC26X2R1 Interface

The CC26X2R1-ZNP uses RX/TX/RTS/CTS for UART communication. See 2.1.2.4 Signal Description for details.

2.1.1.1 Pin Configurations

The CC26X2R1-ZNP pin configurations are described in the following sections.

Default pin configuration

By default, the pin configurations are the following:

Transport CC26X2-ZNP signal CC26X2 PIN CC26X2 NAME Direction
UART TX IOID_3 IOID_3 Out
UART RX IOID_2 IOID_2 In
UART GND GND GND In/Out
Optional pin configuration

If NPI_FLOW_CTRL is enabled then the following pins also apply:

Transport CC26X2-ZNP signal CC26X2 PIN CC26X2 NAME Direction
UART CTS IOID_19 IOID_19 In
UART RTS IOID_18 IOID_18 Out

2.1.2 UART Transport

2.1.2.1 Configuration

The following UART configuration is supported:

  • Baud rate: 115200
  • CTS/RTS flow control with NPI_FLOW_CTRL enabled (not by default)
  • 8-N-1 byte format.
2.1.2.2 Frame Format

UART transport frame format is shown in the following figure. The left-most field is transmitted first over the wire. This is the same General Serial Packet defined by the ZStack Monitor and Test API.

image4

Figure : 2 UART Transport Frame Format

SOF: Start of frame indicator. This is always set to 0xFE.

General frame format: This is the general frame format as described in 2.1.3 General Frame Format.

FCS: Frame-check sequence. This field is computed as an XOR of all the bytes in the general format frame fields.

2.1.2.3 Sample FCS Calculation

Shown below is a C example for the FCS calculation:

unsigned char calcFCS(unsigned char *pMsg, unsigned char len)
{
  unsigned char result = 0;
  while (len--)
  {
    result ^= *pMsg++;
  }
  return result;
}
2.1.2.4 Signal Description

The following standard UART signals are used:

  • TX: Transmit data.
  • RX: Receive data.
  • CTS: Clear to send.
  • RTS: Ready to send.

Figure below shows the RTS/CTS flow control connections to the host processor. On the CC26X2R1, RTS and CTS are active-low signals. The RT output is driven low when the receive register is empty and reception is enabled. Transmission of a byte does not occur before the CTS input is low.

image2

Figure 3 : RTS/CTS Flow Control Connections

2.1.2.5 Signal Operation

UART transport sends and receives data asynchronously. Data can be sent and received simultaneously and the transfer of a frame can be initiated at any time by either the application processor or the ZNP SoC.

2.1.3 General Frame Format

The general frame format is shown in the following figure. The left-most field is transmitted first over the wire. For multi-byte fields, the lowest order byte is transmitted first. This is the same General Frame Format defined by the ZStack Monitor and Test API.

image5

Figure : 4 General Frame Format

Length: The length of the data field of the frame. The length can range from 0-250.

Command: The command of the frame.

Data: The frame data. This depends on the command field and is described for each command in 3. ZNP software command interface.

2.1.3.1 Command Field

The command field is constructed of two bytes. The bytes are formatted as shown in the following figure. The Cmd0 byte is transmitted first.

image6

Figure 5 : Command Field

Type: The command type has one of the following values:

  • 0: POLL. For CC26X2R1, this command type is not supported.
  • 1: SREQ: A synchronous request that requires an immediate response. For example, a function call with a return value would use an SREQ command.
  • 2: AREQ: An asynchronous request. For example, a callback event or a function call with no return value would use an AREQ command.
  • 3: SRSP: A synchronous response. This type of command is only sent in response to a SREQ command. For an SRSP command the subsystem and ID are set to the same values as the corresponding SREQ. The length of an SRSP is generally nonzero, so an SRSP with length=0 can be used to indicate an error.
  • 4-7: Reserved.

Subsystem: The subsystem of the command. Values are shown below:

Subsystem Value Subsystem Name
0 RPC Error interface
1 SYS interface
2 Reserved
3 Reserved
4 AF interface
5 ZDO interface
6 Simple API interface
7 UTIL interface
8 Reserved
9 APP Interface
10-31 Reserved

ID: The command ID. The ID maps to a particular interface message. Value range: 0-255.

When the ZNP cannot recognize an SREQ command from the host processor, the following SRSP is returned:

SRSP:

1 1 1 1 1 1
Length = 0x03 Cmd0 = 0x60 Cmd1 = 0x00 ErrorCode ReqCmd0 ReqCmd1

Attributes:

Attribute Length (byte) Description
ErrorCode 1

The error code maps to one of the following enumerated values.

Value Description
0x01 Invalid subsystem
0x02 Invalid command ID
0x03 Invalid parameter
0x04 Invalid length
ReqCmd0 1 The Cmd0 value of the processed SREQ
ReqCmd1 1 The Cmd1 value of the processed SREQ

2.1.4 Initialization Procedures

2.1.4.1 CC26X2R1-ZNP power-up procedure

The recommended power-up procedure is as follows:

  1. Application processor and CC26X2R1 power up.
  2. The application processor initializes its UART interface.
  3. The application processor receives the SYS_RESET_IND message.

The CC26X2R1-ZNP can be reset when the application processor sends a SYS_RESET_REQ message.

3. ZNP software command interface

The ZNP software command interface is sub-divided into the following categories

  • The SYS interface (MT_SYS) provides the application processor with a low level interface to the ZNP hardware and software.
  • The AF (MT_AF) and ZDO (MT_ZDO) interfaces feature the complete ZigBee interface and can be used to create a full range of ZigBee compliant applications. The AF (Application Framework) interface allows the application processor to register its application with the ZNP and send and receive data. The ZDO (ZigBee Device Object) interface provides various ZigBee management functions like device and service discovery.
  • The UTIL (MT_UTIL) interface provides support functionalities such as setting PAN-ID, getting device info, getting NV info, subscribing callbacks…etc.
  • The APP CONF (MT_APP_CNF) interface provides support for BDB functionality such as set Install Codes, Primary or Secondary Channel, trigger different commissioning methods and other Trust Center configurations.

For further details on the MT interface, refer to the ZStack Monitor and Test API

3.1 Configuration interface

The ZNP device has numerous parameters that can be configured by the application processor. These configuration parameters are stored in non volatile memory on the ZNP device and their values persist across a device reset.

The configuration parameters are divided into “network-specific” and “device-specific” parameters. The “network-specific” configuration parameters should be set to the same value for all ZNP devices in a ZigBee network to ensure proper network operation. The “device-specific” parameters can be set to different values on each device. These parameters are listed in detail in 3.1.1 Device specific configuration parameters and 3.1.2 Network specific configuration parameters. These configuration parameters must be written in Nv for which the host processor must use the MT interface to write Nv parameters into the ZNP device. Refer to the ZStack Monitor and Test API for further details on how to write into Nv.

When the ZNP device powers up, it reads two of the configuration parameters immediately. These are the STARTOPT_CLEAR_CONFIG bit (part of the ZCD_NV_STARTUP_OPTION parameter) and the ZCD_NV_LOGICAL_TYPE parameters. Any modification of these parameters will require a ZNP device reset before they can take effect.

3.1.1 Device specific configuration parameters

3.1.1.1 ZCD_NV_STARTUP_OPTION

Configuration ID: 0x0003; Size: 1 byte; Default value: 0

This parameter controls the device startup options. This is a bit mask of the following values

Bit position 7 6-2 1 0
Description ZCD_STARTOPT_CLEAR_NWK_FRAME_COUNTER Reserved STARTOPT_CLEAR_STATE STARTOPT_CLEAR_CONFIG
  • ZCD_STARTOPT_CLEAR_NWK_FRAME_COUNTER – If this option is set, then the network frame counter is cleared for all networks.

    Note: This should be use only for debug purposes as the network frame counters must be persistant, even after Factory New resets. The usage of this option during the operation in the networks may lead to undesaried behaviour, such as get the ZNP device ignored by other devices in the network.

  • STARTOPT_CLEAR_CONFIG – If this option is set, the device will overwrite all the configuration parameters (except this one) with the “default” values that it is programmed with. This is used to erase the existing configuration and bring the device into a known state.

    Note: The STARTOPT_CLEAR_CONFIG bit is read by the ZNP device immediately when it powers up after a reset.

    When the configuration parameters are restored to defaults, the ZCD_NV_STARTUP_OPTION itself is not restored except for clearing the STARTOPT_CLEAR_CONFIG bit.

  • STARTOPT_CLEAR_STATE – If this option is set, the device will clear its previous network state (which would exist if the device had been operating on a network prior to the reset). This is typically used during application development. During regular device operation, this flag is typically not set, so that an accidental device reset will not cause loss of network state.

    Notes: The ZNP device has two kinds of information stored in non-volatile memory. The configuration parameters (listed in this section) and network state information.

    The configuration parameters are configured by the user before start of ZigBee operation.

    The network state information is collected by the device after it joins a network and creates bindings etc. (at runtime). This is not set by the application processor. This information is stored so that if the device were to reset accidentally, it can restore itself without going through all the network joining and binding process again.

    If the application processor does not wish to continue operating in the previous ZigBee network, it needs to instruct the ZNP device to clear the network state information and start again based on the configuration parameters. This is done by setting the STARTOPT_CLEAR_STATE bit in the startup option.

3.1.1.2 ZCD_NV_LOGICAL_TYPE

Configuration ID: 0x0087; Size: 1 byte; Default value: 0x00

This is the logical type of the device in the ZigBee network. This can be set to a COORDINATOR (0x00), ROUTER (0x01) or ENDDEVICE (0x02).

Note: This parameter is read by the ZNP device immediately when it powers up after a reset.

3.1.1.3 ZCD_NV_ZDO_DIRECT_CB

Configuration ID: 0x008F; Size: 1 byte; Default value: FALSE

This configures the manner in which ZDO responses (hereby referred to as callbacks) are issued to the host processor. By default, this item is set to FALSE, which means that the host processor must use the ZDO_MSG_CB_REGISTER command to subscribe to a specific ZDO callback in order to receive it. The ZDO callback is then conveyed as part of the ZDO_MSG_CB_INCOMING command. If ZCD_NV_ZDO_DIRECT_CB is set TRUE, then the host processor will receive the “verbose” response. For example, the host processor would receive the ZDO_IEEE_ADDR_RSP command in response to ZDO_IEEE_ADDR_REQ.

3.1.2 Network specific configuration parameters

3.1.2.1 ZCD_NV_PANID

Configuration ID: 0x0083; Size: 2 bytes; Default value: 0xFFFF

This parameter identifies the ZigBee network. This should be set to a value between 0 and 0x3FFF. Networks that exist in the same vicinity must have different values for this parameter. It can be set to a special value of 0xFFFF to indicate “don’t care”.

3.2 Z-Stack 3.0 ZNP considerations

3.2.1 Backward compatibility

ZNP is backward compatible with non Z3.0 devices by using the same API that already existed in previous releases of the stack, or by using Base Device Behavior commissioning MT interface with exception of the new security schemas for Z3.0 such as Distributed networks or Install Codes.

3.2.2 ZNP for Z3.0

While the ZNP implementation provides a compatible baseline for ZigBee 3.0 devices, a full implementation of a ZigBee 3.0 device involves additional layers on top of the ZNP. These layers shall be implemented by the user on the host-side of the stack, since they are outside the scope of the network processor. The ZNP provides several new interfaces to enable the required functionality on the host.

In order to update a legacy ZNP-based device to support ZigBee 3.0, the following main updates need to be implemented on the host:

Base Device Behavior Specification:

  1. Finding and Binding: Host processor is required to implement Finding and Binding commissioning method (either as Initiator or as Target) according to the cluster supported by the host application.Touchlink (optional): proximity-based commissioning method.

Green Power Basic proxy:

  1. ZigBee 3.0 coordinator and router devices must implement Green Power Basic proxy functionality. ZNP includes the necessary GP Stub interfaces which are available to the application and allow it to implement GP basic proxy functionality on the host processor.

3.2.3 ZNP startup procedure for Z3.0 implementation

After executing the power-up procedure, the host processor must call some mandatory APIs before executing any APIs that invoke ZigBee over-the-air messaging. Not following this sequence could result in unexpected behaviour. The recommended startup procedure is as follows:

  1. The host processor must use the ZB_WRITE_CONFIGURATION command to configure at the minimum the ZCD_NV_LOGICAL_TYPE
  2. If logical device is defined as ZC or ZR, GP basic proxy must be initialized in the host processor (No ZNP commands are required until interaction with GP devices are needed).
  3. Optional configurations to commission the device are:
    1. Set the Primary and/or Secondary channel mask to perform Formation or Network Steering.
    2. Set the PAN ID to create or join by setting ZCD_NV_PAN_ID.
    3. Set Install codes for networks which require it.
  4. AF_REGISTER command should be sent by the host processor to register the application endpoint.
  5. Host should use BDB commissioning API to create or join the network via standard network formation or joining.
  6. The host processor should wait for BDB notifications on the different commissioning methods used by the host. Also host processor can rely on the supported ZDO states reported.

Example Message Exchange

The following sequence chart is provided as a simple example of a message exchange between a Host and ZNP. In this example the following (generalized) events take place:

  1. The ZNP is reset.
  2. The host writes some configuration data to the ZNP into Nv (ZCD_NV_LOGICAL_TYPE) which will define the logical device role.
  3. An endpoint in the host is registered with the ZNP.
  4. ZNP device is instructed to start a commissioning method according to the device role defined in step 2 (e.g. Commissioning Formation for ZC or ZR, or Commissioning Network Steering for ZR or ZED).
  5. BDB reports the result of the process of the commissioning method execution.
  6. Another device joins the network, indicated by the ZDO Device indications.
  7. Data is exchanged between the Host+ZNP and joining device through AF Data Req’s and AF Incoming Messages.

image3

Figure 6 : Example Message Sequence Chart

3.3 Return Values

The status parameter that is returned from the ZNP device may take one of the following values:

Name Value
ZSuccess 0x00
Zfailure 0x01
ZinvalidParameter 0x02
NV_ITEM_UNINIT 0x09
NV_OPER_FAILED 0x0a
NV_BAD_ITEM_LEN 0x0c
ZmemError 0x10
ZbufferFull 0x11
ZunsupportedMode 0x12
ZmacMemError 0x13
zdoInvalidRequestType 0x80
zdoInvalidEndpoint 0x82
zdoUnsupported 0x84
zdoTimeout 0x85
zdoNoMatch 0x86
zdoTableFull 0x87
zdoNoBindEntry 0x88
ZsecNoKey 0xa1
ZsecMaxFrmCount 0xa3
ZapsFail 0xb1
ZapsTableFull 0xb2
ZapsIllegalRequest 0xb3
ZapsInvalidBinding 0xb4
ZapsUnsupportedAttrib 0xb5
ZapsNotSupported 0xb6
ZapsNoAck 0xb7
ZapsDuplicateEntry 0xb8
ZapsNoBoundDevice 0xb9
ZnwkInvalidParam 0xc1
ZnwkInvalidRequest 0xc2
ZnwkNotPermitted 0xc3
ZnwkStartupFailure 0xc4
ZnwkTableFull 0xc7
ZnwkUnknownDevice 0xc8
ZnwkUnsupportedAttribute 0xc9
ZnwkNoNetworks 0xca
ZnwkLeaveUnconfirmed 0xcb
ZnwkNoAck 0xcc
ZnwkNoRoute 0xcd
ZMacNoACK 0xe9

3.4 Additional considerations for ZNP device in Z-Stack 3.0

  1. The current version of ZNP device does not support commissioning GP devices in the network if these devices require the basic proxy device to switch channel during this commissioning process. Other commissioning methods require that a Host process drives the commissioning process in the application level.

3.5 Additional Information

For additional details of the individual commands, please refer to the ZStack Monitor and Test API.

4 General Information

4.1 Document History

Table 1: Document History

Revision Date Description/Changes
1.0 10/24/2017 Initial version
1.1 5/2/2018 Migrated to new docs