SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.65
Simplifies the implementation of Internet connectivity
SlWlanUpdateProfile_t Struct Reference

Data Fields

_i16 SecType
 
_u8 SsidLen
 
_u8 Priority
 
_u8 Bssid [6]
 
_u8 PasswordLen
 
_u8 WepKeyId
 
_u32 Index
 
_u8 UserLen
 
_u8 AnonUserLen
 
_u8 CertIndex
 
_u8 padding
 
_u32 EapBitmask
 

Detailed Description

Definition at line 601 of file protocol.h.

Field Documentation

§ AnonUserLen

_u8 AnonUserLen

Definition at line 610 of file protocol.h.

§ Bssid

_u8 Bssid[6]

Definition at line 605 of file protocol.h.

§ CertIndex

_u8 CertIndex

Definition at line 611 of file protocol.h.

§ EapBitmask

_u32 EapBitmask

Definition at line 613 of file protocol.h.

§ Index

_u32 Index

Definition at line 608 of file protocol.h.

§ padding

_u8 padding

Definition at line 612 of file protocol.h.

§ PasswordLen

_u8 PasswordLen

Definition at line 606 of file protocol.h.

§ Priority

_u8 Priority

Definition at line 604 of file protocol.h.

§ SecType

_i16 SecType

Definition at line 602 of file protocol.h.

§ SsidLen

_u8 SsidLen

Definition at line 603 of file protocol.h.

§ UserLen

_u8 UserLen

Definition at line 609 of file protocol.h.

§ WepKeyId

_u8 WepKeyId

Definition at line 607 of file protocol.h.


The documentation for this struct was generated from the following file: