SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.65
Simplifies the implementation of Internet connectivity
SlWlanAddGetEapProfile_t Struct Reference

Data Fields

SlWlanAddGetProfile_t Common
 
_u8 UserLen
 
_u8 AnonUserLen
 
_u8 CertIndex
 
_u8 padding
 
_u32 EapBitmask
 

Detailed Description

Definition at line 591 of file protocol.h.

Field Documentation

§ AnonUserLen

_u8 AnonUserLen

Definition at line 594 of file protocol.h.

§ CertIndex

_u8 CertIndex

Definition at line 595 of file protocol.h.

§ Common

Definition at line 592 of file protocol.h.

§ EapBitmask

_u32 EapBitmask

Definition at line 597 of file protocol.h.

§ padding

_u8 padding

Definition at line 596 of file protocol.h.

§ UserLen

_u8 UserLen

Definition at line 593 of file protocol.h.


The documentation for this struct was generated from the following file: