SimpleLink CC31xx/CC32xx Host Driver  Version 3.0.1.65
Simplifies the implementation of Internet connectivity
SlSocketAddrAsyncIPv6EUI48Response_t Struct Reference

Data Fields

_i16 StatusOrLen
 
_u8 Sd
 
_u8 Family
 
_u16 Port
 
_u8 Address [6]
 

Detailed Description

Definition at line 805 of file protocol.h.

Field Documentation

§ Address

_u8 Address[6]

Definition at line 811 of file protocol.h.

§ Family

_u8 Family

Definition at line 809 of file protocol.h.

§ Port

_u16 Port

Definition at line 810 of file protocol.h.

§ Sd

_u8 Sd

Definition at line 808 of file protocol.h.

§ StatusOrLen

_i16 StatusOrLen

Definition at line 807 of file protocol.h.


The documentation for this struct was generated from the following file: