![]() |
![]() |
Functions | |
VAD_API VAD_Handle | VAD_setup () |
VAD_API int_least16_t | VAD_getInitFrames (VAD_Handle handle) |
VAD_API void | VAD_setInitFrames (VAD_Handle handle, int_least16_t initFrames) |
VAD_API int_least16_t | VAD_getDelayFrames (VAD_Handle handle) |
VAD_API void | VAD_setDelayFrames (VAD_Handle handle, int_least16_t delayFrames) |
VAD_API int_least16_t | VAD_getAlpha (VAD_Handle handle) |
VAD_API void | VAD_setAlpha (VAD_Handle handle, int_least16_t alpha) |
VAD_API int_least16_t | VAD_getFastCoef (VAD_Handle handle) |
VAD_API void | VAD_setFastCoef (VAD_Handle handle, int_least16_t fastCoef) |
VAD_API int_least16_t | VAD_getSlowCoef (VAD_Handle handle) |
VAD_API void | VAD_setSlowCoef (VAD_Handle handle, int_least16_t slowCoef) |
VAD_API int_least16_t | VAD_getSignalFloor (VAD_Handle handle) |
VAD_API void | VAD_setSignalFloor (VAD_Handle handle, int_least32_t signalFloor) |
VAD_API int_least16_t | VAD_getNoiseFloor (VAD_Handle handle) |
VAD_API void | VAD_setNoiseFloor (VAD_Handle handle, int_least32_t noiseFloor) |
VAD_API int_least16_t | VAD_getSigSNRThresh (VAD_Handle handle) |
VAD_API void | VAD_setSigSNRThresh (VAD_Handle handle, int_least16_t sigSNRThresh) |
VAD_API int_least16_t | VAD_getSigSNRLimit (VAD_Handle handle) |
VAD_API void | VAD_setSigSNRLimit (VAD_Handle handle, int_least16_t sigSNRLimit) |
VAD_API int_least16_t | VAD_getNoiseRate (VAD_Handle handle) |
VAD_API void | VAD_setNoiseRate (VAD_Handle handle, int_least16_t noiseRate) |
VAD_API VAD_MessageEnum | VAD_run (VAD_Handle handle, int_least16_t rmsegy) |
VAD_API const char * | VAD_getVersion (void) |
Functions of the VAD API
VAD_API VAD_Handle VAD_setup | ( | ) |
Initialize the VAD object prior to starting detection. Prepares the VAD object to start detecting audio events. It must be called before any other VAD functions including get/set functions. Returns handle to VAD object.
VAD_API int_least16_t VAD_getInitFrames | ( | VAD_Handle | handle | ) |
Gets the initialization stabilization duration in frames. Get initialization stabilization duration in frames.
[in] | handle | VAD handle |
VAD_API void VAD_setInitFrames | ( | VAD_Handle | handle, |
int_least16_t | initFrames | ||
) |
Sets the the initialization stabilization duration in frames. Set initialization stabilization duration in frames.
0 < initFrames <= INT16_MAX
[in] | handle | VAD handle |
[in] | initFrames | Initialization frames |
VAD_API int_least16_t VAD_getDelayFrames | ( | VAD_Handle | handle | ) |
Gets number of sequential frames above noise to declare activity. Get sequential frames above noise to declare activity.
[in] | handle | VAD handle |
VAD_API void VAD_setDelayFrames | ( | VAD_Handle | handle, |
int_least16_t | delayFrames | ||
) |
Sets number of sequential frames above noise to declare activity. Set sequential frames above noise to declare activity.
0 < delayFrames <= INT16_MAX
[in] | handle | VAD handle |
[in] | delayFrames | Delay frames |
VAD_API int_least16_t VAD_getAlpha | ( | VAD_Handle | handle | ) |
Gets smoothed signal energy filter coefficient alpha. Get smoothed signal energy filter coefficient alpha
[in] | handle | VAD handle |
VAD_API void VAD_setAlpha | ( | VAD_Handle | handle, |
int_least16_t | alpha | ||
) |
Sets smoothed signal energy filter coefficient alpha. Set smoothed signal energy filter coefficient alpha (Q15).
0 < alpha <= INT16_MAX
[in] | handle | VAD handle |
[in] | alpha | Smoothing filter coefficient alpha |
VAD_API int_least16_t VAD_getFastCoef | ( | VAD_Handle | handle | ) |
Gets fast activity estimator filter coefficient. Get fast activity estimator filter coefficient (Q15).
[in] | handle | VAD handle |
VAD_API void VAD_setFastCoef | ( | VAD_Handle | handle, |
int_least16_t | fastCoef | ||
) |
Sets fast activity estimator filter coefficient. Set fast activity estimator filter coefficient (Q15).
0 < fastCoef <= INT16_MAX
[in] | handle | VAD handle |
[in] | fastCoef | Fast activity estimator filter coefficient; |
VAD_API int_least16_t VAD_getSlowCoef | ( | VAD_Handle | handle | ) |
Gets slow activity estimator filter coefficient. Gets slow activity estimator filter coefficient (Q15).
[in] | handle | VAD handle |
VAD_API void VAD_setSlowCoef | ( | VAD_Handle | handle, |
int_least16_t | slowCoef | ||
) |
Sets slow activity estimator filter coefficient. Set slow activity estimator filter coefficient (Q15).
0 < slowCoef <= INT16_MAX
[in] | handle | VAD handle |
[in] | slowCoef | Slow activity estimator filter coefficient; |
VAD_API int_least16_t VAD_getSignalFloor | ( | VAD_Handle | handle | ) |
Gets signal RMS energy floor.
[in] | handle | VAD handle |
VAD_API void VAD_setSignalFloor | ( | VAD_Handle | handle, |
int_least32_t | signalFloor | ||
) |
Sets signal RMS energy floor. Set signal RMS energy floor in (Q30).
0 < signalFloor <= INT32_MAX
[in] | handle | VAD handle |
[in] | signalFloor | Signal rms energy floor in (Q30); |
VAD_API int_least16_t VAD_getNoiseFloor | ( | VAD_Handle | handle | ) |
Gets noise RMS energy floor. Gets noise RMS energy floor in (Q30).
[in] | handle | VAD handle |
VAD_API void VAD_setNoiseFloor | ( | VAD_Handle | handle, |
int_least32_t | noiseFloor | ||
) |
Sets noise RMS energy floor. Set noise RMS energy floor in (Q30).
0 < noiseFloor <= INT32_MAX
[in] | handle | VAD handle |
[in] | noiseFloor | Noise RMS energy floor in (Q30); |
VAD_API int_least16_t VAD_getSigSNRThresh | ( | VAD_Handle | handle | ) |
Gets signal SNR threshold. Get signal SNR threshold (Q10)
[in] | handle | VAD handle |
VAD_API void VAD_setSigSNRThresh | ( | VAD_Handle | handle, |
int_least16_t | sigSNRThresh | ||
) |
Sets signal SNR threshold. Sets signal SNR threshold (Q10).
0 < sigSNRThresh <= INT16_MAX
[in] | handle | VAD handle |
[in] | sigSNRThresh | Signal SNR threshold (Q10); |
VAD_API int_least16_t VAD_getSigSNRLimit | ( | VAD_Handle | handle | ) |
Gets signal SNR Limit. Get signal SNR Limit (Q10)
[in] | handle | VAD handle |
VAD_API void VAD_setSigSNRLimit | ( | VAD_Handle | handle, |
int_least16_t | sigSNRLimit | ||
) |
Sets signal SNR limit. Set signal SNR limit (Q10).
0 < sigSNRLimit <= INT16_MAX
[in] | handle | VAD handle |
[in] | sigSNRLimit | SNR limit (Q10) |
VAD_API int_least16_t VAD_getNoiseRate | ( | VAD_Handle | handle | ) |
Get noise floor maximum upward adaptation rate multiplier (Q14). Gets noise floor maximum upward adaptation rate multiplier (Q14).
[in] | handle | VAD handle |
VAD_API void VAD_setNoiseRate | ( | VAD_Handle | handle, |
int_least16_t | noiseRate | ||
) |
Set noise floor maximum upward adaptation rate multiplier. Sets noise floor maximum upward adaptation rate multiplier (Q14).
0 < noiseRate <= INT16_MAX
[in] | handle | VAD handle |
[in] | noiseRate | Noise maximum upward rate (Q14); |
VAD_API VAD_MessageEnum VAD_run | ( | VAD_Handle | handle, |
int_least16_t | rmsegy | ||
) |
Performs voice activity detection. Runs the voice activity detector for one frame returning result. The declaration that speech is found will be delayed by delayFrames seconds from when speech actually started. The parameter rmsegy is the average rms energy in the frame of data in Q15, normalized to a peak rms energy of 1.0 (32767 in Q15). For each frame, VAD returns a message indicating the status of the VAD result. During non-speech it returns VAD_Background. When it detects some signal above the background noise it returns VAD_Hang. If this continues long enough to declare a speech signal found it will return VAD_Detect for one frame. Thereafter, as long as the speech signal continues, it will return VAD_Ongoing. At the end of the utterance it will return to VAD_Background.
[in] | handle | VAD handle |
[in] | rmsegy | Normalized frame RMS energy (Q15) |
VAD_API const char* VAD_getVersion | ( | void | ) |
Get VAD library version number.