LittlevGL  3.20.00.19
Data Fields
lv_img_dsc_t Struct Reference

#include <lv_img_decoder.h>

Collaboration diagram for lv_img_dsc_t:
Collaboration graph
[legend]

Data Fields

lv_img_header_t header
 
uint32_t data_size
 
const uint8_t * data
 

Detailed Description

Image header it is compatible with the result from image converter utility

Field Documentation

§ header

lv_img_header_t lv_img_dsc_t::header

§ data_size

uint32_t lv_img_dsc_t::data_size

§ data

const uint8_t* lv_img_dsc_t::data

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale