Go to the source code of this file.
§ LV_HOR_RES
The horizontal resolution of the currently active display.
§ LV_VER_RES
The vertical resolution of the currently active display.
§ lv_disp_get_scr_act()
Return with a pointer to the active screen
- Parameters
-
| disp | pointer to display which active screen should be get. (NULL to use the default screen) |
- Returns
- pointer to the active screen object (loaded by 'lv_scr_load()')
§ lv_disp_load_scr()
Make a screen active
- Parameters
-
§ lv_disp_get_layer_top()
Return with the top layer. (Same on every screen and it is above the normal screen layer)
- Parameters
-
| disp | pointer to display which top layer should be get. (NULL to use the default screen) |
- Returns
- pointer to the top layer object (transparent screen sized lv_obj)
§ lv_disp_get_layer_sys()
Return with the sys. layer. (Same on every screen and it is above the normal screen and the top layer)
- Parameters
-
| disp | pointer to display which sys. layer should be get. (NULL to use the default screen) |
- Returns
- pointer to the sys layer object (transparent screen sized lv_obj)
§ lv_disp_assign_screen()
Assign a screen to a display.
- Parameters
-
| disp | pointer to a display where to assign the screen |
| scr | pointer to a screen object to assign |
§ lv_disp_get_refr_task()
Get a pointer to the screen refresher task to modify its parameters with lv_task_... functions.
- Parameters
-
- Returns
- pointer to the display refresher task. (NULL on error)
§ lv_disp_get_inactive_time()
| uint32_t lv_disp_get_inactive_time |
( |
const lv_disp_t * |
disp | ) |
|
Get elapsed time since last user activity on a display (e.g. click)
- Parameters
-
| disp | pointer to an display (NULL to get the overall smallest inactivity) |
- Returns
- elapsed ticks (milliseconds) since the last activity
§ lv_disp_trig_activity()
| void lv_disp_trig_activity |
( |
lv_disp_t * |
disp | ) |
|
Manually trigger an activity on a display
- Parameters
-
| disp | pointer to an display (NULL to use the default display) |