xWRL6432 MMWAVE-L-SDK  05.05.00.00
mpdProc_ClusterParamCfg Struct Reference

Data Fields

uint16_t enabled
 Configure clustering logic. 0 - disabled 1 – enabled. More...
 
float maxDistance
 The radius (in meters) of the neighborhood around a point (i.e., epsilon in DBSCAN algorithm). More...
 
uint16_t minPoints
 
More...
 

Field Documentation

◆ enabled

uint16_t mpdProc_ClusterParamCfg::enabled

Configure clustering logic. 0 - disabled 1 – enabled.

◆ maxDistance

float mpdProc_ClusterParamCfg::maxDistance

The radius (in meters) of the neighborhood around a point (i.e., epsilon in DBSCAN algorithm).

◆ minPoints

uint16_t mpdProc_ClusterParamCfg::minPoints