AoAProcHWA DPU Object.
The structure is used to hold AoAProcHWA internal data object
Data Fields | |
DPU_AoAProcHWA_InitParams | initParms |
AoAProc_dpParams | params |
Data path common parameters used in aoaProc. More... | |
HWA_Handle | hwaHandle |
EDMA Handle. More... | |
EDMA_Handle | edmaHandle |
EDMA Handle. More... | |
DPU_AoAProcHWA_HwaCfg | hwaCfg |
aoaProc HWA configuration More... | |
DPU_AoAProc_Edma | edmaIn_rangeFFT |
aoaProc HWA configuration before Doppler FFT is applied More... | |
DPU_AoAProc_Edma | edmaIn_dopplerFFT |
aoaProc HWA configuration before AoA FFT's are applied More... | |
SemaphoreP_Object | edmaDoneSemaHandle |
aoaProc HWA data input paramset trigger */ uint8_t dataInTriggerRangeFFT[2]; More... | |
SemaphoreP_Object | hwaDoneSemaHandleDopp |
HWA Processing Done (Doppler) semaphore Handle. More... | |
SemaphoreP_Object | hwaDoneSemaHandleAoA |
HWA Processing Done (AoA) semaphore Handle. More... | |
cmplx16ImRe_t * | radarCubebuf |
Pointer to Radar Cube buffer. More... | |
uint32_t | hwaMemBankAddr [SOC_HWA_NUM_MEM_BANKS] |
HWA Memory address. More... | |
bool | inProgress |
AoAProc DPU is in processing state. More... | |
uint32_t | numProcess |
Total number of AoAProc DPU processing. More... | |
uint8_t | hwaDmaTriggerDoppPing |
DMA trigger source channel (before Doppler FFT) for Ping param set. More... | |
uint8_t | hwaDmaTriggerDoppPong |
DMA trigger source channel (before Doppler FFT) for Pong param set. More... | |
uint8_t | hwaDmaTriggerAoAPing |
DMA trigger source channel (before AoA FFT) for Ping param set. More... | |
uint8_t | hwaDmaTriggerAoAPong |
DMA trigger source channel (before AoA FFT) for Pong param set. More... | |
uint16_t | hwaDoppNumLoops |
HWA number of loops for Doppler FFT and compensation. More... | |
uint16_t | hwaDoppNumLoops1 |
HWA number (1-basically if the no. is odd) of loops for Doppler FFT and compensation. More... | |
uint16_t | hwaAoANumLoops |
HWA number of loops for AoA and max of Elevation-Azimuth FFT. More... | |
uint16_t | hwaAoANumLoops1 |
HWA number (1-basically if the no. is odd) of loops for AoA and max of Elevation-Azimuth FFT. More... | |
uint8_t | hwaParamStartIdxDopp |
HWA start paramset index - Doppler FFT and compensation. More... | |
uint8_t | hwaParamStopIdxDopp |
HWA stop paramset index - Doppler FFT and compensation. More... | |
uint8_t | hwaParamStartIdxAoA |
HWA start paramset index - AoA Calculation. More... | |
uint8_t | hwaParamStopIdxAoA |
HWA stop paramset index - AoA Calculation. More... | |
uint16_t * | rangeGatesCount |
Doppler FFT to be run on those range gates which have a maximum in first 50-points. More... | |
DPU_AoAProc_Edma | edmaOut_maxAoA |
aoaProc EDMA configuration AoA FFT's are applied More... | |
SemaphoreP_Object | hwaSemaHandleParamset |
HWA Paramset Done semaphore Handle for ping/pong in Doppler use case. More... | |
cmplx16ImRe_t * | angleMatBuf |
Pointer to Angle Matrix buffer. More... | |
uint16_t * | hwaAoANumLoops |
HWA number of loops for AoA and max of Elevation-Azimuth FFT. More... | |
uint16_t * | range_idx_arr |
Array to store range index for which Doppler FFT is to be applied. More... | |
uint16_t * | angle_idx_doppler_count_arr |
Array to store Doppler index corresponding to range index for which Angle FFT is to be applied. More... | |
int16_t * | doppler_idx_arr |
Array to store Doppler index corresponding to range index for which Angle FFT is to be applied. More... | |
cmplx32ImRe_t * | antenna_array |
Antenna array to store elements before applying elevation-azimuth FFT. More... | |
uint8_t | numTxAntennas |
Number of transmit antennas. More... | |
uint8_t | doppFFT_is16b |
Flag to set Doppler FFT to 16-bit(1-True)/32-bit(0-False) More... | |
uint8_t | numVirtualAntennas |
Number of virtual antennas. More... | |
uint8_t | max_num_points |
Number of max points under consideration. More... | |
uint8_t | antenna_array_elements |
Number of max points under consideration. More... | |
uint8_t * | isDopplerPhaseCompensationEnabled |
Flag to check Doppler compensations is enabled or not. More... | |
DPU_AoAProcHWA_InitParams aoaProcHWAObj::initParms |
AoAProc_dpParams aoaProcHWAObj::params |
Data path common parameters used in aoaProc.
HWA_Handle aoaProcHWAObj::hwaHandle |
EDMA Handle.
EDMA_Handle aoaProcHWAObj::edmaHandle |
EDMA Handle.
EDMA Handle of TPCC B.
DPU_AoAProcHWA_HwaCfg aoaProcHWAObj::hwaCfg |
aoaProc HWA configuration
DPU_AoAProc_Edma aoaProcHWAObj::edmaIn_rangeFFT |
aoaProc HWA configuration before Doppler FFT is applied
aoaProc EDMA configuration before Doppler FFT is applied
DPU_AoAProc_Edma aoaProcHWAObj::edmaIn_dopplerFFT |
aoaProc HWA configuration before AoA FFT's are applied
aoaProc EDMA configuration before AoA FFT's are applied
SemaphoreP_Object aoaProcHWAObj::edmaDoneSemaHandle |
aoaProc HWA data input paramset trigger */ uint8_t dataInTriggerRangeFFT[2];
EDMA done semaphore.
/*! aoaProc HWA data output paramset trigger */ uint8_t dataOutTriggerMaxN[2];
/*! @brief EDMA done semaphore
SemaphoreP_Object aoaProcHWAObj::hwaDoneSemaHandleDopp |
HWA Processing Done (Doppler) semaphore Handle.
SemaphoreP_Object aoaProcHWAObj::hwaDoneSemaHandleAoA |
HWA Processing Done (AoA) semaphore Handle.
cmplx16ImRe_t * aoaProcHWAObj::radarCubebuf |
Pointer to Radar Cube buffer.
uint32_t aoaProcHWAObj::hwaMemBankAddr |
HWA Memory address.
bool aoaProcHWAObj::inProgress |
AoAProc DPU is in processing state.
uint32_t aoaProcHWAObj::numProcess |
Total number of AoAProc DPU processing.
uint8_t aoaProcHWAObj::hwaDmaTriggerDoppPing |
DMA trigger source channel (before Doppler FFT) for Ping param set.
uint8_t aoaProcHWAObj::hwaDmaTriggerDoppPong |
DMA trigger source channel (before Doppler FFT) for Pong param set.
uint8_t aoaProcHWAObj::hwaDmaTriggerAoAPing |
DMA trigger source channel (before AoA FFT) for Ping param set.
uint8_t aoaProcHWAObj::hwaDmaTriggerAoAPong |
DMA trigger source channel (before AoA FFT) for Pong param set.
uint16_t aoaProcHWAObj::hwaDoppNumLoops |
HWA number of loops for Doppler FFT and compensation.
uint16_t aoaProcHWAObj::hwaDoppNumLoops1 |
HWA number (1-basically if the no. is odd) of loops for Doppler FFT and compensation.
uint16_t aoaProcHWAObj::hwaAoANumLoops |
HWA number of loops for AoA and max of Elevation-Azimuth FFT.
uint16_t aoaProcHWAObj::hwaAoANumLoops1 |
HWA number (1-basically if the no. is odd) of loops for AoA and max of Elevation-Azimuth FFT.
uint8_t aoaProcHWAObj::hwaParamStartIdxDopp |
HWA start paramset index - Doppler FFT and compensation.
uint8_t aoaProcHWAObj::hwaParamStopIdxDopp |
HWA stop paramset index - Doppler FFT and compensation.
uint8_t aoaProcHWAObj::hwaParamStartIdxAoA |
HWA start paramset index - AoA Calculation.
uint8_t aoaProcHWAObj::hwaParamStopIdxAoA |
HWA stop paramset index - AoA Calculation.
uint16_t * aoaProcHWAObj::rangeGatesCount |
Doppler FFT to be run on those range gates which have a maximum in first 50-points.
DPU_AoAProc_Edma aoaProcHWAObj::edmaOut_maxAoA |
aoaProc EDMA configuration AoA FFT's are applied
SemaphoreP_Object aoaProcHWAObj::hwaSemaHandleParamset |
HWA Paramset Done semaphore Handle for ping/pong in Doppler use case.
cmplx16ImRe_t* aoaProcHWAObj::angleMatBuf |
Pointer to Angle Matrix buffer.
uint16_t* aoaProcHWAObj::hwaAoANumLoops |
HWA number of loops for AoA and max of Elevation-Azimuth FFT.
uint16_t* aoaProcHWAObj::range_idx_arr |
Array to store range index for which Doppler FFT is to be applied.
uint16_t* aoaProcHWAObj::angle_idx_doppler_count_arr |
Array to store Doppler index corresponding to range index for which Angle FFT is to be applied.
int16_t* aoaProcHWAObj::doppler_idx_arr |
Array to store Doppler index corresponding to range index for which Angle FFT is to be applied.
cmplx32ImRe_t* aoaProcHWAObj::antenna_array |
Antenna array to store elements before applying elevation-azimuth FFT.
uint8_t aoaProcHWAObj::numTxAntennas |
Number of transmit antennas.
uint8_t aoaProcHWAObj::doppFFT_is16b |
Flag to set Doppler FFT to 16-bit(1-True)/32-bit(0-False)
uint8_t aoaProcHWAObj::numVirtualAntennas |
Number of virtual antennas.
uint8_t aoaProcHWAObj::max_num_points |
Number of max points under consideration.
uint8_t aoaProcHWAObj::antenna_array_elements |
Number of max points under consideration.
uint8_t* aoaProcHWAObj::isDopplerPhaseCompensationEnabled |
Flag to check Doppler compensations is enabled or not.