xWRL6432 MMWAVE-L-SDK  05.05.00.00
DPU_DoaProc_HwaCfg Struct Reference

Detailed Description

dopplerProc DPU HWA configuration parameters

The structure is used to hold the HWA configuration parameters for the Doppler Processing DPU

Data Fields

uint8_t winSym
 Indicates if HWA window is symmetric or non-symmetric. Use HWA macro definitions for symmetric/non-symmetric. More...
 
uint32_t windowSize
 Doppler FFT window size in bytes. This is the number of coefficients to be programmed in the HWA for the windowing functionality. The size is a function of numDopplerChirps as follows:
If non-symmetric window is selected: windowSize = numDopplerChirps * sizeof(int32_t)
If symmetric window is selected and numDopplerChirps is even: windowSize = numDopplerChirps * sizeof(int32_t) / 2
If symmetric window is selected and numDopplerChirps is odd: windowSize = (numDopplerChirps + 1) * sizeof(int32_t) / 2
More...
 
int32_t * window
 Pointer to Doppler FFT window coefficients. More...
 
uint32_t winRamOffset
 HWA window RAM offset in number of samples. More...
 
uint8_t firstStageScaling
 Indicates if HWA should enable butterfly scaling (divide by 2) of the first radix-2 stage. Depending on the window definition, user may want to skip the first stage scaling in order to avoid signal degradation.
Options are:
Disable first stage scaling: firstStageScaling = DPU_DOAPROC_FIRST_SCALING_DISABLED
Enable first stage scaling: firstStageScaling = DPU_DOAPROC_FIRST_SCALING_ENABLED
Note: All other butterfly stages have the scaling enabled. This option applies only for the first stage.
. More...
 
uint8_t numParamSets
 Number of HWA paramsets reserved for the Doppler DPU. The number of HWA paramsets required by this DPU is a function of the number of TX antennas used in the configuration:
numParamSets = 2 x (Number of TX antennas) + 2
The DPU will use numParamSets consecutively, starting from paramSetStartIdx.
. More...
 
uint32_t paramSetStartIdx
 HWA paramset Start index.
Application has to ensure that paramSetStartIdx is such that
[paramSetStartIdx, paramSetStartIdx + 1, ... (paramSetStartIdx + numParamSets - 1)]
is a valid set of HWA paramsets.
. More...
 
uint32_t hwaMemInpAddr
 HWA input memory bank address. More...
 
DPU_DoaProc_HWA_Option_Cfg doaRngGateCfg
 HWA Doppler FFT Parmas set configuration (performing Doppler FFT and antenna mapping) More...
 
uint8_t dmaTrigSrcChan
 HWA param set dma trigger source channel. More...
 

Field Documentation

◆ winSym

uint8_t DPU_DoaProc_HwaCfg::winSym

Indicates if HWA window is symmetric or non-symmetric. Use HWA macro definitions for symmetric/non-symmetric.

◆ windowSize

uint32_t DPU_DoaProc_HwaCfg::windowSize

Doppler FFT window size in bytes. This is the number of coefficients to be programmed in the HWA for the windowing functionality. The size is a function of numDopplerChirps as follows:
If non-symmetric window is selected: windowSize = numDopplerChirps * sizeof(int32_t)
If symmetric window is selected and numDopplerChirps is even: windowSize = numDopplerChirps * sizeof(int32_t) / 2
If symmetric window is selected and numDopplerChirps is odd: windowSize = (numDopplerChirps + 1) * sizeof(int32_t) / 2

◆ window

int32_t* DPU_DoaProc_HwaCfg::window

Pointer to Doppler FFT window coefficients.

◆ winRamOffset

uint32_t DPU_DoaProc_HwaCfg::winRamOffset

HWA window RAM offset in number of samples.

◆ firstStageScaling

uint8_t DPU_DoaProc_HwaCfg::firstStageScaling

Indicates if HWA should enable butterfly scaling (divide by 2) of the first radix-2 stage. Depending on the window definition, user may want to skip the first stage scaling in order to avoid signal degradation.
Options are:
Disable first stage scaling: firstStageScaling = DPU_DOAPROC_FIRST_SCALING_DISABLED
Enable first stage scaling: firstStageScaling = DPU_DOAPROC_FIRST_SCALING_ENABLED
Note: All other butterfly stages have the scaling enabled. This option applies only for the first stage.
.

◆ numParamSets

uint8_t DPU_DoaProc_HwaCfg::numParamSets

Number of HWA paramsets reserved for the Doppler DPU. The number of HWA paramsets required by this DPU is a function of the number of TX antennas used in the configuration:
numParamSets = 2 x (Number of TX antennas) + 2
The DPU will use numParamSets consecutively, starting from paramSetStartIdx.
.

◆ paramSetStartIdx

uint32_t DPU_DoaProc_HwaCfg::paramSetStartIdx

HWA paramset Start index.
Application has to ensure that paramSetStartIdx is such that
[paramSetStartIdx, paramSetStartIdx + 1, ... (paramSetStartIdx + numParamSets - 1)]
is a valid set of HWA paramsets.
.

◆ hwaMemInpAddr

uint32_t DPU_DoaProc_HwaCfg::hwaMemInpAddr

HWA input memory bank address.

◆ doaRngGateCfg

DPU_DoaProc_HWA_Option_Cfg DPU_DoaProc_HwaCfg::doaRngGateCfg

HWA Doppler FFT Parmas set configuration (performing Doppler FFT and antenna mapping)

◆ dmaTrigSrcChan

uint8_t DPU_DoaProc_HwaCfg::dmaTrigSrcChan

HWA param set dma trigger source channel.