xWRL6432 MMWAVE-L-SDK  05.05.00.00
DPU_AoAProcHWA_HW_Resources Struct Reference

Detailed Description

AoA DPU HW configuration parameters.

The structure is used to hold the HW configuration parameters for the AoA DPU

Data Fields

DPU_AoAProcHWA_EdmaCfg edmaCfg
 EDMA configuration. More...
 
DPU_AoAProcHWA_HwaCfg hwaCfg
 HWA configuration. More...
 
DPIF_RadarCube radar_1D_FFT_Cube
 Radar Cube. More...
 
DPIF_Anglemat angleMat
 Angle Matrix on which Elevation-Azimuth FFT is to be applied. More...
 
uint32_t * maxVal_elev_azim
 Matrix where the azimuth-elevation FFT max values is stored (this matrix should be in M4 for ease of computation. More...
 
Edma_IntrObjectintrObj
 EDMA interrupt object. More...
 

Field Documentation

◆ edmaCfg

DPU_AoAProcHWA_EdmaCfg DPU_AoAProcHWA_HW_Resources::edmaCfg

EDMA configuration.

◆ hwaCfg

DPU_AoAProcHWA_HwaCfg DPU_AoAProcHWA_HW_Resources::hwaCfg

HWA configuration.

◆ radar_1D_FFT_Cube

DPIF_RadarCube DPU_AoAProcHWA_HW_Resources::radar_1D_FFT_Cube

Radar Cube.

◆ angleMat

DPIF_Anglemat DPU_AoAProcHWA_HW_Resources::angleMat

Angle Matrix on which Elevation-Azimuth FFT is to be applied.

◆ maxVal_elev_azim

uint32_t* DPU_AoAProcHWA_HW_Resources::maxVal_elev_azim

Matrix where the azimuth-elevation FFT max values is stored (this matrix should be in M4 for ease of computation.

◆ intrObj

Edma_IntrObject* DPU_AoAProcHWA_HW_Resources::intrObj

EDMA interrupt object.