PINMUX Driver API/interface file.
This file contains pad configure register offsets and bit-field value macros for different configurations,
BIT[21] TXDISABLE disable the pin's output driver BIT[18] RXACTIVE enable the pin's input buffer (typically kept enabled) BIT[17] PULLTYPESEL set the iternal resistor pull direction high or low (if enabled) BIT[16] PULLUDEN internal resistor disable (0 = enabled / 1 = disabled) BIT[3:0] MUXMODE select the desired function on the given pin
Go to the source code of this file.
Data Structures | |
struct | Pinmux_PerCfg_t |
Structure defining the pin configuration parameters. More... | |
struct | PadToPin_t |
Macros | |
#define | PINMUX_END (0xFFFFFFFFU) |
Macro to mark end of pinmux config array. More... | |
#define | PIN_MODE(mode) (mode) |
Pin mode. More... | |
#define | PIN_PULL_DISABLE (0x1U << 8U) |
Resistor disable. More... | |
#define | PIN_PULL_DIRECTION (0x1U << 9U) |
Pull direction, 0: pull-down, 1: pull-up. More... | |
Pinmux Domain ID | |
#define | PINMUX_DOMAIN_ID_MAIN (0U) |
NOT USED on this SOC. More... | |
#define | PINMUX_DOMAIN_ID_MCU (1U) |
NOT USED on this SOC. More... | |
Pad config register offset in control module | |
#define | PIN_PAD_AA (0x00000000U) |
#define | PIN_PAD_AB (0x00000004U) |
#define | PIN_PAD_AC (0x00000008U) |
#define | PIN_PAD_AD (0x0000000CU) |
#define | PIN_PAD_AE (0x00000010U) |
#define | PIN_PAD_AF (0x00000014U) |
#define | PIN_PAD_AG (0x00000018U) |
#define | PIN_PAD_AH (0x0000001CU) |
#define | PIN_PAD_AI (0x00000020U) |
#define | PIN_PAD_AJ (0x00000024U) |
#define | PIN_PAD_AK (0x00000028U) |
#define | PIN_PAD_AL (0x0000002CU) |
#define | PIN_PAD_AM (0x00000030U) |
#define | PIN_PAD_AN (0x00000034U) |
#define | PIN_PAD_AO (0x00000038U) |
#define | PIN_PAD_AP (0x0000003CU) |
#define | PIN_PAD_AQ (0x00000040U) |
#define | PIN_PAD_AR (0x00000044U) |
#define | PIN_PAD_AS (0x00000048U) |
#define | PIN_PAD_AT (0x0000004CU) |
#define | PIN_PAD_AU (0x00000050U) |
#define | PIN_PAD_AV (0x00000054U) |
#define | PIN_PAD_AW (0x00000058U) |
#define | PIN_PAD_AX (0x0000005CU) |
#define | PIN_OVERRIDE_INPUT_ENABLE (0x1U << 5U) |
Pin Input Override. More... | |
#define | PIN_OVERRIDE_INPUT_ENABLE_CTRL (0x1U << 4U) |
#define | PIN_OVERRIDE_OUTPUT_DISABLE (0x1U << 7U) |
Pin Output Override. More... | |
#define | PIN_OVERRIDE_OUTPUT_DISABLE_CTRL (0x1U << 6U) |
#define | PIN_SLEW_RATE_HIGH (0x0U << 10U) |
Slew Rate High. More... | |
#define | PIN_SLEW_RATE_LOW (0x1U << 10U) |
Slew Rate Low. More... | |
Functions | |
void | Pinmux_config (const Pinmux_PerCfg_t *pinmuxCfg, uint32_t domainId) |
This API configures the pinmux based on the domain. More... | |
uint32_t | Pinmux_Read (uint32_t pinOffset) |
uint32_t | Pinmux_getMode (uint32_t pad) |
uint32_t | Pinmux_getPinNum (uint32_t pad) |
void | Pinmux_inputoverride (uint32_t offset, bool state) |
This API is used to override input enable. More... | |
void | Pinmux_outputoverride (uint32_t offset, bool state) |
This API configures pin output override. More... | |