Return status | |
#define | SystemP_SUCCESS ((int32_t )0) |
Return status when the API execution was successful. More... | |
#define | SystemP_FAILURE ((int32_t)-1) |
Return status when the API execution was not successful due to a failure. More... | |
#define | SystemP_TIMEOUT ((int32_t)-2) |
Return status when the API execution failed due to a time out. More... | |
#define | SystemP_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters. More... | |
#define | SystemP_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy. More... | |
#define | SystemP_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid LLD state. More... | |
#define | SystemP_OUT_OF_RESOURCES ((int32_t)-6) |
Return status when the API execution failed due to lack of resources (memory / HW) More... | |
Timeout values | |
#define | SystemP_NO_WAIT ((uint32_t)0) |
Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More... | |
#define | SystemP_WAIT_FOREVER ((uint32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available. More... | |
#define SystemP_SUCCESS ((int32_t )0) |
Return status when the API execution was successful.
#define SystemP_FAILURE ((int32_t)-1) |
Return status when the API execution was not successful due to a failure.
#define SystemP_TIMEOUT ((int32_t)-2) |
Return status when the API execution failed due to a time out.
#define SystemP_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters.
#define SystemP_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy.
#define SystemP_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid LLD state.
#define SystemP_OUT_OF_RESOURCES ((int32_t)-6) |
Return status when the API execution failed due to lack of resources (memory / HW)
#define SystemP_NO_WAIT ((uint32_t)0) |
Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available.
#define SystemP_WAIT_FOREVER ((uint32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available.