Go to the source code of this file.
Data Structures | |
struct | DebugP_ShmLog |
Data structure describing log in shared memory. More... | |
Macros | |
#define | DebugP_SHM_LOG_SIZE ( (2U*1024U) - 16U) |
size of shared memory log for a CPU More... | |
#define | DebugP_MEM_LOG_SIZE ( 4U*1024U ) |
size of memory log for a CPU More... | |
#define | DebugP_SHM_LOG_IS_VALID (0x12345678U) |
Flag to indicate shared memory buffer is valid. More... | |
Debug log zones | |
#define | DebugP_LOG_ZONE_ALWAYS_ON (0x0001U) |
Flag for always on zone, enabled by default and recommend to not switch off. More... | |
#define | DebugP_LOG_ZONE_ERROR (0x0002U) |
Flag for error zone. More... | |
#define | DebugP_LOG_ZONE_WARN (0x0004U) |
Flag for warning zone. More... | |
#define | DebugP_LOG_ZONE_INFO (0x0008U) |
Flag for info zone. More... | |
Compile time log and assert enable, disable | |
#define | DebugP_ASSERT_ENABLED 1 |
Pre-processor define to enable or disable DebugP assert's. More... | |
#define | DebugP_LOG_ENABLED 1 |
Pre-processor define to enable or disable DebugP log's. More... | |
Debug assert APIs | |
#define | DebugP_assert(expression) _DebugP_assert(expression, __FILE__, __FUNCTION__, __LINE__, #expression) |
Function to call for assert check. More... | |
#define | DebugP_assertNoLog(expression) (_DebugP_assertNoLog(expression)) |
Function to call for assert check, no logs are printed. More... | |
Debug log APIs | |
#define | DebugP_log(format, ...) _DebugP_logZone(DebugP_LOG_ZONE_ALWAYS_ON, format, ##__VA_ARGS__) |
Function to log a string to the enabled console. More... | |
#define | DebugP_logError(format, ...) _DebugP_logZone(DebugP_LOG_ZONE_ERROR, "ERROR: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__) |
Function to log a string to the enabled console, for error zone. More... | |
#define | DebugP_logWarn(format, ...) _DebugP_logZone(DebugP_LOG_ZONE_WARN, "WARNING: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__) |
Function to log a string to the enabled console, for warning zone. More... | |
#define | DebugP_logInfo(format, ...) _DebugP_logZone(DebugP_LOG_ZONE_INFO, "INFO: %s:%d: " format, __FUNCTION__, __LINE__, ##__VA_ARGS__) |
Function to log a string to the enabled console, for info zone. More... | |
Functions | |
void | _DebugP_assert (int expression, const char *file, const char *function, int line, const char *expressionString) |
Actual function that is called for assert's by DebugP_assert. More... | |
void | _DebugP_assertNoLog (int expression) |
Actual function that is called for assert's by DebugP_assertNoLog. More... | |
void | _DebugP_logZone (uint32_t logZone, char *format,...) |
Function to log a string to the enabled console for a given zone. More... | |
void | DebugP_logChar (char a) |
Function to log a char to the enabled console. More... | |
uint32_t | DebugP_logZoneEnable (uint32_t logZoneMask) |
Enable log zones. More... | |
uint32_t | DebugP_logZoneDisable (uint32_t logZoneMask) |
Disable log zones. More... | |
void | DebugP_shmLogWriterPutLine (uint8_t *buf, uint16_t num_bytes) |
Write a line to shared memory log. More... | |
void | DebugP_logZoneRestore (uint32_t logZoneMask) |
Restire zone mask returned from DebugP_logZoneDisable or DebugP_logZoneEnable. More... | |
void | DebugP_shmLogWriterInit (DebugP_ShmLog *shmLog, uint16_t selfCoreId) |
Initialize shared memory log writer for this core. More... | |
void | DebugP_shmLogWriterPutChar (char character) |
Write a character to shared memory log. More... | |
void | DebugP_uartLogWriterPutChar (char character) |
Write a character to UART terminal. More... | |
void | DebugP_shmLogReaderInit (DebugP_ShmLog *shmLog, uint16_t numCores) |
Initialize log reader to read from shared memory and log to console via DebugP_log. More... | |
void | DebugP_memLogWriterInit (uint16_t selfCoreId) |
Initialize log write to write to memory trace buffer. More... | |
void | DebugP_memTraceLogWriterPutLine (uint8_t *buf, uint16_t num_bytes) |
Write a line to trace buffer. More... | |
void | DebugP_memLogWriterPutChar (char character) |
Write a character to trace buffer. More... | |
void | DebugP_uartSetDrvIndex (uint32_t uartDrvIndex) |
Set UART driver index to use for character read and write form UART. More... | |
int32_t | DebugP_scanf (char *format,...) |
Read a formatted string from the selected UART driver. More... | |
int32_t | DebugP_readLine (char *lineBuf, uint32_t bufSize) |
Read a string from the selected UART driver. More... | |