Data Fields | |
uint16_t | pointThre1 |
Number of detected points (in a single frame) needed in a zone to enter the motion/presence state. If the number of points exceed this threshold, no need to check the SNR. More... | |
uint16_t | pointThre2 |
Number of detected points (in a single frame) needed in a zone to enter the motion/presence state. If the number of points exceeds this threshold, the snrThre2 criteria is checked. More... | |
float | snrThre2 |
Minimum total SNR (linear) of detected points (in a single frame) in a zone to enter the motion/presence state if the pointThre2 criteria is also satisfied. More... | |
uint16_t | pointHistThre1 |
Number of detected points (in a frame history buffer) needed in a zone to enter the motion/presence state. If the number of points exceed this threshold, no need to check the SNR. More... | |
uint16_t | pointHistThre2 |
Number of detected points (in a frame history buffer) needed in a zone to enter the motion/presence state. If the number of points exceeds this threshold, the snrHistThre2 criteria is checked. More... | |
float | snrHistThre2 |
Minimum total SNR (linear) of detected points (in a frame history buffer) in a zone to enter the motion/presence state if the pointHistThre2 criteria is also satisfied. More... | |
uint16_t | histBufferSize |
Size of the frame history buffer size (in frames) used in pointHistThre1, pointHistThre2, and snrHistThre2 parameters. More... | |
uint16_t | stateExitThre |
A motion status is preserved if it recorded at least one motion detection in the last major2minorThre frames. More... | |
uint16_t mpdProc_MotionModeStateParamCfg::pointThre1 |
Number of detected points (in a single frame) needed in a zone to enter the motion/presence state. If the number of points exceed this threshold, no need to check the SNR.
uint16_t mpdProc_MotionModeStateParamCfg::pointThre2 |
Number of detected points (in a single frame) needed in a zone to enter the motion/presence state. If the number of points exceeds this threshold, the snrThre2 criteria is checked.
float mpdProc_MotionModeStateParamCfg::snrThre2 |
Minimum total SNR (linear) of detected points (in a single frame) in a zone to enter the motion/presence state if the pointThre2 criteria is also satisfied.
uint16_t mpdProc_MotionModeStateParamCfg::pointHistThre1 |
Number of detected points (in a frame history buffer) needed in a zone to enter the motion/presence state. If the number of points exceed this threshold, no need to check the SNR.
uint16_t mpdProc_MotionModeStateParamCfg::pointHistThre2 |
Number of detected points (in a frame history buffer) needed in a zone to enter the motion/presence state. If the number of points exceeds this threshold, the snrHistThre2 criteria is checked.
float mpdProc_MotionModeStateParamCfg::snrHistThre2 |
Minimum total SNR (linear) of detected points (in a frame history buffer) in a zone to enter the motion/presence state if the pointHistThre2 criteria is also satisfied.
uint16_t mpdProc_MotionModeStateParamCfg::histBufferSize |
Size of the frame history buffer size (in frames) used in pointHistThre1, pointHistThre2, and snrHistThre2 parameters.
uint16_t mpdProc_MotionModeStateParamCfg::stateExitThre |
A motion status is preserved if it recorded at least one motion detection in the last major2minorThre frames.