Data Fields | |
uint16_t | enabled |
Configure clustering logic. 0 - disabled 1 – enabled. More... | |
float | maxDistance |
The radius (in meters) of the neighborhood around a point (i.e., epsilon in DBSCAN algorithm). More... | |
uint16_t | minPoints |
More... | |
uint16_t mpdProc_ClusterParamCfg::enabled |
Configure clustering logic. 0 - disabled 1 – enabled.
float mpdProc_ClusterParamCfg::maxDistance |
The radius (in meters) of the neighborhood around a point (i.e., epsilon in DBSCAN algorithm).
uint16_t mpdProc_ClusterParamCfg::minPoints |