EDMA Parameter RAM Set in User Configurable format This is a mapping of the EDMA PaRAM set provided to the user for ease of modification of the individual fields.
Data Fields | |
uint32_t | opt |
uint32_t | srcAddr |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address. More... | |
uint16_t | aCnt |
uint16_t | bCnt |
uint32_t | destAddr |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0. More... | |
int16_t | srcBIdx |
int16_t | destBIdx |
uint16_t | linkAddr |
Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking. More... | |
uint16_t | bCntReload |
Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers. More... | |
int16_t | srcCIdx |
int16_t | destCIdx |
uint16_t | cCnt |
int8_t | srcBIdxExt |
int8_t | destBIdxExt |
uint32_t __attribute__::opt |
uint32_t __attribute__::srcAddr |
Starting byte address of Source For FIFO mode, srcAddr must be a 256-bit aligned address.
uint16_t __attribute__::aCnt |
uint16_t __attribute__::bCnt |
uint32_t __attribute__::destAddr |
Starting byte address of destination For FIFO mode, destAddr must be a 256-bit aligned address. i.e. 5 LSBs should be 0.
int16_t __attribute__::srcBIdx |
int16_t __attribute__::destBIdx |
uint16_t __attribute__::linkAddr |
Address for linking (AutoReloading of a PaRAM Set) This must point to a valid aligned 32-byte PaRAM set A value of 0xFFFF means no linking.
uint16_t __attribute__::bCntReload |
Reload value of the numArrInFrame (BCNT) Relevant only for A-sync transfers.
int16_t __attribute__::srcCIdx |
int16_t __attribute__::destCIdx |
uint16_t __attribute__::cCnt |
int8_t __attribute__::srcBIdxExt |
int8_t __attribute__::destBIdxExt |