xWRL6432 MMWAVE-L-SDK  05.04.00.01

Detailed Description

Parameters for TimerP_setup.

Data Fields

uint32_t inputPreScaler
 
uint32_t inputClkHz
 
uint32_t periodInUsec
 
uint32_t oneshotMode
 
uint32_t enableOverflowInt
 

Field Documentation

◆ inputPreScaler

uint32_t TimerP_Params::inputPreScaler

input pre-scaler divisor ro apply

NOTE MUST be power of 2 and between 1 and 256 for GP Timer NOTE MAKE sure this value is not 0

◆ inputClkHz

uint32_t TimerP_Params::inputClkHz

Timer input clock in unit of Hz before pre-scaler, system initialization MUST make any system level muxes, PLLs, power required to input this clock are setup properly

NOTE MAKE sure this value is not 0

◆ periodInUsec

uint32_t TimerP_Params::periodInUsec

Timer period in units of usecs, internally TimerP_Params::inputClkHz and TimerP_Params.inputPreScaler is used to compute the value to be put inside the timer HW register

NOTE MAKE sure this value is not 0

◆ oneshotMode

uint32_t TimerP_Params::oneshotMode

0: continous mode of operation, 1: oneshot mode of operation

◆ enableOverflowInt

uint32_t TimerP_Params::enableOverflowInt

0: Do not enable timer overflow interrupt, 1: enable timer overflow interrupt