Flash device attributes, these are filled by SysCfg based on the flash device that is selected.
Data Fields | |
uint32_t | flashType |
char * | flashName |
uint32_t | deviceId |
uint32_t | manufacturerId |
uint32_t | driverInstance |
uint32_t | flashSize |
uint32_t | blockCount |
uint32_t | blockSize |
uint32_t | pageCount |
uint32_t | pageSize |
uint32_t | sectorCount |
uint32_t | sectorSize |
uint32_t Flash_Attrs::flashType |
Flash type. Whether it's NAND or NOR
char* Flash_Attrs::flashName |
Flash name. Taken from Sysconfig
uint32_t Flash_Attrs::deviceId |
Flash device ID as read form the flash device, this will be filled when Flash_open() is called
uint32_t Flash_Attrs::manufacturerId |
Flash manufacturer ID as read form the flash device, this will be filled when Flash_open() is called
uint32_t Flash_Attrs::driverInstance |
Underlying OSPI peripheral driver instance that is used by the flash driver, e.g OSPI driver
uint32_t Flash_Attrs::flashSize |
Flash size, in bytes
uint32_t Flash_Attrs::blockCount |
Number of blocks in the flash the flash
uint32_t Flash_Attrs::blockSize |
Size of each block, in bytes
uint32_t Flash_Attrs::pageCount |
Number of pages per block
uint32_t Flash_Attrs::pageSize |
Size of each page, in bytes
uint32_t Flash_Attrs::sectorCount |
Number of sectors in the flash, if flash supports sectors
uint32_t Flash_Attrs::sectorSize |
Size of each flash sector, in bytes