Doppler DPU static configuration parameters.
The structure is used to hold the static configuration parameters for the DOA DPU.
Data Fields | |
uint8_t | numTxAntennas |
Number of transmit antennas. More... | |
uint8_t | numRxAntennas |
Number of receive antennas. More... | |
uint8_t | numVirtualAntennas |
Number of virtual antennas. More... | |
uint16_t | numRangeBins |
Number of range bins. More... | |
uint16_t | numDopplerChirps |
Number of Doppler chirps. More... | |
uint16_t | numDopplerBins |
Number of Doppler bins. More... | |
uint16_t | azimuthFftSize |
Azimuth FFT size. More... | |
uint16_t | elevationFftSize |
elevation FFT size More... | |
uint16_t | numMinorMotionChirpsPerFrame |
Number of chirps per frame for Minor Motion Detection. More... | |
uint16_t | numFrmPerMinorMotProc |
Number of frames Minor Motion Detection spreads over. More... | |
uint8_t | log2NumDopplerBins |
Log2 of number of Doppler bins. More... | |
uint8_t | selectCoherentPeakInDopplerDim |
true - select the coherent peak in Doppler, false - non-coherently combine accross Doppler More... | |
uint8_t | angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas More... | |
bool | isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format. More... | |
bool | isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg. More... | |
bool | isRxChGainPhaseCompensationEnabled |
Range Bias and rx channel gain/phase compensation enable flag. More... | |
DPU_DoaProc_compRxChannelBiasCfg | compRxChanCfg |
Range Bias and rx channel gain/phase compensation configuration. More... | |
uint16_t | doaRangeLoopType |
Range loop type: 0 - HWA internal loop, 1- Loop controlled by CPU. More... | |
bool | enableMajorMotion |
Major motion detection enable flag. More... | |
bool | enableMinorMotion |
Minor motion detection enable flag. More... | |
uint16_t | numAntRow |
Number of virtual antenna rows. More... | |
uint16_t | numAntCol |
Number of virtual antenna columns. More... | |
uint8_t DPU_DoaProc_StaticConfig::numTxAntennas |
Number of transmit antennas.
uint8_t DPU_DoaProc_StaticConfig::numRxAntennas |
Number of receive antennas.
uint8_t DPU_DoaProc_StaticConfig::numVirtualAntennas |
Number of virtual antennas.
uint16_t DPU_DoaProc_StaticConfig::numRangeBins |
Number of range bins.
uint16_t DPU_DoaProc_StaticConfig::numDopplerChirps |
Number of Doppler chirps.
uint16_t DPU_DoaProc_StaticConfig::numDopplerBins |
Number of Doppler bins.
uint16_t DPU_DoaProc_StaticConfig::azimuthFftSize |
Azimuth FFT size.
uint16_t DPU_DoaProc_StaticConfig::elevationFftSize |
elevation FFT size
uint16_t DPU_DoaProc_StaticConfig::numMinorMotionChirpsPerFrame |
Number of chirps per frame for Minor Motion Detection.
uint16_t DPU_DoaProc_StaticConfig::numFrmPerMinorMotProc |
Number of frames Minor Motion Detection spreads over.
uint8_t DPU_DoaProc_StaticConfig::log2NumDopplerBins |
Log2 of number of Doppler bins.
uint8_t DPU_DoaProc_StaticConfig::selectCoherentPeakInDopplerDim |
true - select the coherent peak in Doppler, false - non-coherently combine accross Doppler
uint8_t DPU_DoaProc_StaticConfig::angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas
bool DPU_DoaProc_StaticConfig::isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format.
bool DPU_DoaProc_StaticConfig::isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg.
bool DPU_DoaProc_StaticConfig::isRxChGainPhaseCompensationEnabled |
Range Bias and rx channel gain/phase compensation enable flag.
DPU_DoaProc_compRxChannelBiasCfg DPU_DoaProc_StaticConfig::compRxChanCfg |
Range Bias and rx channel gain/phase compensation configuration.
uint16_t DPU_DoaProc_StaticConfig::doaRangeLoopType |
Range loop type: 0 - HWA internal loop, 1- Loop controlled by CPU.
bool DPU_DoaProc_StaticConfig::enableMajorMotion |
Major motion detection enable flag.
bool DPU_DoaProc_StaticConfig::enableMinorMotion |
Minor motion detection enable flag.
uint16_t DPU_DoaProc_StaticConfig::numAntRow |
Number of virtual antenna rows.
uint16_t DPU_DoaProc_StaticConfig::numAntCol |
Number of virtual antenna columns.