Source and destination addresses for EDMA input configuration.
The structure is one of the input arguments of the DPU's proces function.
Data Fields | |
uint32_t | srcAddress |
Address in L3 of the chunk of data in radar cube matrix to be copied to HWA More... | |
uint32_t | dstAddress |
Destination address in HWA of the copied chunk. More... | |
uint32_t | Bcnt_Acnt |
Packed EDMA values for A count (LSB 16-bit position) and B count (MSB 16-bit position. More... | |
uint32_t DPU_DoaProc_RadarCubeChunkEdmaCfg::srcAddress |
Address in L3 of the chunk of data in radar cube matrix to be copied to HWA
uint32_t DPU_DoaProc_RadarCubeChunkEdmaCfg::dstAddress |
Destination address in HWA of the copied chunk.
uint32_t DPU_DoaProc_RadarCubeChunkEdmaCfg::Bcnt_Acnt |
Packed EDMA values for A count (LSB 16-bit position) and B count (MSB 16-bit position.