HWA CFAR static configuration.
The structure is used to hold the static configuration used for CFAR. The following condition must be satisfied:
Data Fields | |
uint8_t | log2NumDopplerBins |
Log2 of number of doppler bins. More... | |
uint16_t | numRangeBins |
Number of range bins. More... | |
uint16_t | numDopplerBins |
Number of doppler bins. More... | |
uint16_t | azimuthFftSize |
Azimuth FFT size. More... | |
uint16_t | elevationFftSize |
Elevation FFT size. More... | |
float | rangeStep |
Range conversion factor for FFT range index to meters. More... | |
float | dopplerStep |
Doppler conversion factor for Doppler FFT index to m/s. More... | |
float | lambdaOverDistX |
Lambda over antenna spacing in x-direction. More... | |
float | lambdaOverDistZ |
Lambda over antenna spacing in z-direction. More... | |
float | rangeBias |
Range bias. More... | |
uint8_t | selectCoherentPeakInDopplerDim |
1 - select the coherent peak in Doppler, 0 - non-coherently combine accross Doppler, zero doppler output, 2 - non-coherently combine accross Doppler, doppler output based on Doppler maximum position More... | |
uint8_t | angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas More... | |
uint8_t | detectionHeatmapType |
0-Range-Azimuth heatmap, 1-Range-Doppler heatmap More... | |
bool | isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg. More... | |
bool | isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format. More... | |
bool | enableCfarPointCloudListWithIndices |
enable CFAR point cloud list with range/azimuth indices More... | |
uint8_t DPU_CFARProcHWA_StaticConfig::log2NumDopplerBins |
Log2 of number of doppler bins.
uint16_t DPU_CFARProcHWA_StaticConfig::numRangeBins |
Number of range bins.
uint16_t DPU_CFARProcHWA_StaticConfig::numDopplerBins |
Number of doppler bins.
uint16_t DPU_CFARProcHWA_StaticConfig::azimuthFftSize |
Azimuth FFT size.
uint16_t DPU_CFARProcHWA_StaticConfig::elevationFftSize |
Elevation FFT size.
float DPU_CFARProcHWA_StaticConfig::rangeStep |
Range conversion factor for FFT range index to meters.
float DPU_CFARProcHWA_StaticConfig::dopplerStep |
Doppler conversion factor for Doppler FFT index to m/s.
float DPU_CFARProcHWA_StaticConfig::lambdaOverDistX |
Lambda over antenna spacing in x-direction.
float DPU_CFARProcHWA_StaticConfig::lambdaOverDistZ |
Lambda over antenna spacing in z-direction.
float DPU_CFARProcHWA_StaticConfig::rangeBias |
Range bias.
uint8_t DPU_CFARProcHWA_StaticConfig::selectCoherentPeakInDopplerDim |
1 - select the coherent peak in Doppler, 0 - non-coherently combine accross Doppler, zero doppler output, 2 - non-coherently combine accross Doppler, doppler output based on Doppler maximum position
uint8_t DPU_CFARProcHWA_StaticConfig::angleDimension |
1 - 1D: 6x1 azimuth antenna array 2 - 2D: one lower row: 4 antennas, upper row 2 antennas
uint8_t DPU_CFARProcHWA_StaticConfig::detectionHeatmapType |
0-Range-Azimuth heatmap, 1-Range-Doppler heatmap
bool DPU_CFARProcHWA_StaticConfig::isStaticClutterRemovalEnabled |
Static Clutter Removal Cfg.
bool DPU_CFARProcHWA_StaticConfig::isDetMatrixLogScale |
Detection matrix format 0 - Linear 32-bit integer, 1 - 16-bit log2 magnitude in Q11 format.
bool DPU_CFARProcHWA_StaticConfig::enableCfarPointCloudListWithIndices |
enable CFAR point cloud list with range/azimuth indices