EDMA configuration for Sync A copy.
The structure is used to hold the sync A configuration
Data Fields | |
uint32_t | srcAddress |
Source Address. More... | |
uint32_t | destAddress |
Destination Address. More... | |
uint16_t | aCount |
a count More... | |
uint16_t | bCount |
b count More... | |
uint16_t | cCount |
c count More... | |
int16_t | srcBIdx |
source B index More... | |
int16_t | dstBIdx |
destination B index More... | |
int16_t | srcCIdx |
source C index More... | |
int16_t | dstCIdx |
destination C index More... | |
uint32_t DPEDMA_syncACfg::srcAddress |
Source Address.
uint32_t DPEDMA_syncACfg::destAddress |
Destination Address.
uint16_t DPEDMA_syncACfg::aCount |
a count
uint16_t DPEDMA_syncACfg::bCount |
b count
uint16_t DPEDMA_syncACfg::cCount |
c count
int16_t DPEDMA_syncACfg::srcBIdx |
source B index
int16_t DPEDMA_syncACfg::dstBIdx |
destination B index
int16_t DPEDMA_syncACfg::srcCIdx |
source C index
int16_t DPEDMA_syncACfg::dstCIdx |
destination C index