EDMA channel configuration.
The structure is used to hold the EDMA channel configuration
Data Fields | |
uint32_t | channel |
EDMA channel id. More... | |
uint32_t | paramId |
EDMA ParamSet triggered by event on channel. More... | |
uint16_t | channelShadow |
EDMA channel shadow id. More... | |
uint32_t | shadowPramId |
EDMA shadow ParamSet id. More... | |
uint32_t | eventQueue |
EDMA event Queue used for the transfer. More... | |
uint32_t | tcc |
EDMA event Queue used for the transfer. More... | |
uint32_t DPEDMA_ChanCfg::channel |
EDMA channel id.
uint32_t DPEDMA_ChanCfg::paramId |
EDMA ParamSet triggered by event on channel.
uint16_t DPEDMA_ChanCfg::channelShadow |
EDMA channel shadow id.
uint32_t DPEDMA_ChanCfg::shadowPramId |
EDMA shadow ParamSet id.
uint32_t DPEDMA_ChanCfg::eventQueue |
EDMA event Queue used for the transfer.
uint32_t DPEDMA_ChanCfg::tcc |
EDMA event Queue used for the transfer.