EDMA channel configuration with 3 shadow channels.
The structure is used to hold the EDMA channel configuration for 1 EDMA channel which is linked to 3 shadow channels.
Data Fields | |
uint32_t | channel |
EDMA channel id. More... | |
uint32_t | paramId |
EDMA ParamSet triggered by event on channel. More... | |
uint32_t | ShadowPramId [3] |
EDMA channel shadow id. More... | |
uint32_t | eventQueue |
EDMA event Queue used for the transfer. More... | |
uint32_t | tcc |
EDMA event Queue used for the transfer. More... | |
uint32_t DPEDMA_3LinkChanCfg::channel |
EDMA channel id.
uint32_t DPEDMA_3LinkChanCfg::paramId |
EDMA ParamSet triggered by event on channel.
uint32_t DPEDMA_3LinkChanCfg::ShadowPramId[3] |
EDMA channel shadow id.
uint32_t DPEDMA_3LinkChanCfg::eventQueue |
EDMA event Queue used for the transfer.
uint32_t DPEDMA_3LinkChanCfg::tcc |
EDMA event Queue used for the transfer.