EDMA channel configuration with 2 shadow channels.
The structure is used to hold the EDMA channel configuration for 1 EDMA channel which is linked to 2 shadow channels.
Data Fields | |
uint8_t | channel |
EDMA channel id. More... | |
uint16_t | channelShadow [2] |
EDMA channel shadow id. More... | |
uint8_t | eventQueue |
EDMA event Queue used for the transfer. More... | |
uint8_t DPEDMA_2LinkChanCfg::channel |
EDMA channel id.
uint16_t DPEDMA_2LinkChanCfg::channelShadow[2] |
EDMA channel shadow id.
uint8_t DPEDMA_2LinkChanCfg::eventQueue |
EDMA event Queue used for the transfer.