Data structure defines the MCAN protocol status.
Data Fields | |
uint32_t | lastErrCode |
uint32_t | act |
uint32_t | errPassive |
uint32_t | warningStatus |
uint32_t | busOffStatus |
uint32_t | dlec |
uint32_t | resi |
uint32_t | rbrs |
uint32_t | rfdf |
uint32_t | pxe |
uint32_t | tdcv |
uint32_t CANFDLLD_MCANProtocolStatus::lastErrCode |
Last Error Code Refer enum CANFDLLD_MCANErrCode
uint32_t CANFDLLD_MCANProtocolStatus::act |
Activity - Monitors the module's CAN communication state. refer enum CANFDLLD_MCANCommState
uint32_t CANFDLLD_MCANProtocolStatus::errPassive |
Error Passive 0 = The M_CAN is in the Error_Active state 1 = The M_CAN is in the Error_Passive state
uint32_t CANFDLLD_MCANProtocolStatus::warningStatus |
Warning Status 0 = Both error counters are below the Error_Warning limit of 96 1 = At least one of error counter has reached the Error_Warning limit of 96
uint32_t CANFDLLD_MCANProtocolStatus::busOffStatus |
Bus_Off Status 0 = The M_CAN is not Bus_Off 1 = The M_CAN is in Bus_Off state
uint32_t CANFDLLD_MCANProtocolStatus::dlec |
Data Phase Last Error Code Refer enum CANFDLLD_MCANErrCode
uint32_t CANFDLLD_MCANProtocolStatus::resi |
ESI flag of last received CAN FD Message 0 = Last received CAN FD message did not have its ESI flag set 1 = Last received CAN FD message had its ESI flag set
uint32_t CANFDLLD_MCANProtocolStatus::rbrs |
BRS flag of last received CAN FD Message 0 = Last received CAN FD message did not have its BRS flag set 1 = TLast received CAN FD message had its BRS flag set
uint32_t CANFDLLD_MCANProtocolStatus::rfdf |
Received a CAN FD Message 0 = Since this bit was reset by the CPU, no CAN FD message has been received 1 = Message in CAN FD format with FDF flag set has been received
uint32_t CANFDLLD_MCANProtocolStatus::pxe |
Protocol Exception Event 0 = No protocol exception event occurred since last read access 1 = Protocol exception event occurred
uint32_t CANFDLLD_MCANProtocolStatus::tdcv |
Transmitter Delay Compensation Value