Data structure defines the MCAN error logging counters status.
Data Fields | |
uint32_t | transErrLogCnt |
uint32_t | recErrCnt |
uint32_t | rpStatus |
uint32_t | canErrLogCnt |
uint32_t CANFDLLD_MCANErrCntStatus::transErrLogCnt |
Transmit Error Counter
uint32_t CANFDLLD_MCANErrCntStatus::recErrCnt |
Receive Error Counter
uint32_t CANFDLLD_MCANErrCntStatus::rpStatus |
Receive Error Passive 0 = The Receive Error Counter is below the error passive level(128) 1 = The Receive Error Counter has reached the error passive level(128)
uint32_t CANFDLLD_MCANErrCntStatus::canErrLogCnt |
CAN Error Logging