Data structure defines the ECC Error Status.
Data Fields | |
uint32_t | secErr |
uint32_t | dedErr |
uint32_t | row |
uint32_t | bit1 |
uint32_t | bit2 |
uint32_t CANFDLLD_MCANECCErrStatus::secErr |
Single Bit Error Status 0 = No Single Bit Error pending 1 = Single Bit Error pending
uint32_t CANFDLLD_MCANECCErrStatus::dedErr |
Double Bit Error Status 0 = No Double Bit Error pending 1 = Double Bit Error pending
uint32_t CANFDLLD_MCANECCErrStatus::row |
Indicates the row/address where the single or double bit error occurred.
uint32_t CANFDLLD_MCANECCErrStatus::bit1 |
Indicates the bit position in the ram data that is in error
uint32_t CANFDLLD_MCANECCErrStatus::bit2 |
Indicates the bit position in the ram data that is in error Valid only in case of DED.