Data structure defines the ECC Error forcing.
Data Fields | |
uint32_t | errType |
uint32_t | rowNum |
uint32_t | bit1 |
uint32_t | bit2 |
uint32_t | errOnce |
uint32_t | errForce |
uint32_t CANFDLLD_MCANECCErrForceParams::errType |
Error type to be forced Refer enum CANFDLLD_MCANECCErrType.
uint32_t CANFDLLD_MCANECCErrForceParams::rowNum |
Row address where error needs to be applied.
uint32_t CANFDLLD_MCANECCErrForceParams::bit1 |
Column/Data bit that needs to be flipped when force_sec or force_ded is set
uint32_t CANFDLLD_MCANECCErrForceParams::bit2 |
Data bit that needs to be flipped when force_ded is set
uint32_t CANFDLLD_MCANECCErrForceParams::errOnce |
Force Error once 1: The error will inject an error to the specified row only once
uint32_t CANFDLLD_MCANECCErrForceParams::errForce |
Force error on the next RAM read